IB_GetBdAddr Function
C
bool IB_GetBdAddr(uint8_t * p_bdAddr);
Description
This routine will get Bluetooth Device Address from IB. If there exists BDADDR IB, then it will return the BDADDR stored in IB. Otherwise, it returns FAILS (1)
Parameters
Param | Description |
---|---|
uint8_t "p_Addr" | the pointer to the memory stores BDADDR |
Returns
A boolean value, True means valid BDADDR IB