IB_GetBdAddr Function

C

bool IB_GetBdAddr(uint8_t * p_bdAddr);

Description

This routine will get Bluetooth Device Address from IB. If there exists BDADDR IB, then it will return the BDADDR stored in IB. Otherwise, it returns FAILS (1)

Parameters

ParamDescription
uint8_t "p_Addr"the pointer to the memory stores BDADDR

Returns

A boolean value, True means valid BDADDR IB