1.1.1.2.1 OSAL_QUEUE_Create Function
C
OSAL_RESULT OSAL_QUEUE_Create(OSAL_QUEUE_HANDLE_TYPE *queID, uint32_t queueLength, uint32_t itemSize);
Description
Creates a new queue instance, and returns a handle by which the new queue can be referenced
Parameters
Param | Description |
---|---|
queID | A pointer to the queue ID |
queueLength | The maximum number of items that the queue can contain. |
itemSize | The number of bytes each item in the queue will require. Items are queued by copy, not by reference, so this is the number of bytes that will be copied for each posted item. Each item in the queue must be the same size. |
Returns
OSAL_RESULT_TRUE - A queue had been created
OSAL_RESULT_FALSE - Queue creation failed