IB_GetMACAddr Function

C

bool IB_GetMACAddr(uint8_t * p_addr);

Description

This routine will get ZB MAC Address from IB. If there exists MAC_ADDR IB, then it will return the MAC_ADDR stored in IB. Otherwise, it returns FAILS (1))

Parameters

ParamDescription
uint8_t "p_Addr"the pointer to the memory stores MAC_ADDR

Returns

A boolean value, True means valid ZB MAC Address IB