6.3.1.4 Reading the value of a GPIO pin
Use the following command to read the value of a GPIO pin.
AT+DIGRD=<Pin>
- Pin: Replace this with the number of the pin that needs to be read.
Use the following command to read the value of a GPIO pin.
AT+DIGRD=<Pin>
Rev: C