1 Harmony 3 Driver and System Service Application Examples for SAM RH707 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
| Name | Description |
|---|---|
| FAT Filesystem using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT Filesystem using SDSPI Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
| I2C Driver Synchronous - I2C EEPROM | This example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM |
| SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
| SPI Driver Synchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |