11 Example
Add this to the main loop or a setup function:
/* Configure push button 0 to trigger an interrupt on falling edge */ioport_set_pin_dir(EXAMPLE_BUTTON_INT, IOPORT_DIR_INPUT);ioport_set_pin_mode(EXAMPLE_BUTTON_INT, IOPORT_MODE_PULLUP |IOPORT_MODE_GLITCH_FILTER);ioport_set_pin_sense_mode(EXAMPLE_BUTTON_INT, IOPORT_SENSE_FALLING);if(!gpio_set_pin_callback(EXAMPLE_BUTTON_INT, pb0_callback, 1)) {printf("Set pin callback failure!\r\n");while(1) {}}gpio_enable_pin_interrupt(EXAMPLE_BUTTON_INT);
- Initialize a pin to trigger an interrupt. Here, we initialize PC03 as an input pin with pull up and glitch filter and to generate an interrupt on a falling edge.
ioport_set_pin_dir(EXAMPLE_BUTTON_INT, IOPORT_DIR_INPUT);ioport_set_pin_mode(EXAMPLE_BUTTON_INT, IOPORT_MODE_PULLUP |IOPORT_MODE_GLITCH_FILTER);ioport_set_pin_sense_mode(EXAMPLE_BUTTON_INT, IOPORT_SENSE_FALLING); - Set a callback for the pin interrupt.
if(!gpio_set_pin_callback(EXAMPLE_BUTTON_INT, pb0_callback, 1)) {printf("Set pin callback failure!\r\n");while(1) {}} - Enable pin interrupt.
gpio_enable_pin_interrupt(EXAMPLE_BUTTON_INT);