10.3.1 NVM User Row Mapping
The first two 32-bit words of the NVM User Row contain calibration data that are automatically read at device power on.
The NVM User Row can be read at address 0x804000.
To write the NVM User Row refer to NVMCTRL – Non-Volatile Memory Controller.
When writing to the user row the values do not get loaded by the other modules on the device until a device reset occurs.
Bit Position | Name | Usage |
---|---|---|
2:0 | BOOTPROT | Used to select one of eight different bootloader sizes. Refer to “NVMCTRL – Non-Volatile Memory Controller”. Default value = 7 except for WLCSP (Default value = 3). |
3 | Reserved | |
6:4 | EEPROM | Used to select one of eight different EEPROM Emulation sizes. Refer to “NVMCTRL – Non-Volatile Memory Controller”. Default value = 7. |
7 | Reserved | |
13:8 | BOD33 Level | BOD33
Threshold Level at power on. Refer to the SYSCTRL BOD33 register.
Default value = 0x7 (non-AECQ100) Default value = 0x22 (AECQ100) |
14 | BOD33 Enable | BOD33 enable at power on. Refer to the SYSCTRL BOD33 register. Default value = 1. |
16:15 | BOD33 Action | BOD33 Action at power on. Refer to the SYSCTRL BOD33 register. Default value = 1. |
24:17 | Reserved | Voltage Regulator Internal BOD (BOD12) configuration. These bits are written in production and must not be changed. Default value = 0x70. |
25 | WDT Enable | WDT Enable at power on. Refer to the WDT CTRL register. Default value = 0. |
26 | WDT Always-On | WDT Always-On at power on. Refer to the WDT CTRL register. Default value = 0. |
30:27 | WDT Period | WDT Period at power on. Refer to the WDT CONFIG register. Default value = 0x0B. |
34:31 | WDT Window | WDT Window mode time-out at power on. Refer to the WDT CONFIG register. Default value = 0x05. |
38:35 | WDT EWOFFSET | WDT Early Warning Interrupt Time Offset at power on. Refer to the WDT EWCTRL register. Default value = 0x0B. |
39 | WDT WEN | WDT Timer Window Mode Enable at power on. Refer to the WDT CTRL register. Default value = 0. |
40 | BOD33 Hysteresis | BOD33 Hysteresis configuration at power on. Refer to the SYSCTRL BOD33 register. Default value = 0. |
41 | Reserved | Voltage Regulator Internal BOD(BOD12) configuration. This bit is written in production and must not be changed. Default value = 0. |
47:42 | Reserved | |
63:48 | LOCK | NVM Region Lock Bits. Refer to “NVMCTRL – Non-Volatile Memory Controller”. Default value = 0xFFFF. |