crypto_Aead_Status_E Crypto_Aead_AesCcm_Cipher(
st_Crypto_Aead_AesCcm_ctx *ptr_aesCcmCtx_st,
crypto_CipherOper_E cipherOper_en,
uint8_t *ptr_inputData,
uint32_t dataLen,
uint8_t *ptr_outData,
uint8_t *ptr_nonce,
uint32_t nonceLen,
uint8_t *ptr_authTag,
uint32_t authTagLen,
uint8_t *ptr_aad,
uint32_t aadLen
);
Description
This API performs AES-CCM encryption or decryption. Before using it, initialize the
context by calling the Crypto_Aead_AesCcm_Init function.
Parameters
| No. | Argument Type | Argument Name | Type | Description |
|---|
| 1 | st_Crypto_Aead_AesCcm_ctx* | ptr_aesCcmCtx_st | Input | AES-CCM
algorithm context. |
| 2 | crypto_CipherOper_E | cipherOper_en | Input | Selection
cipher operation is encryption or decryption. |
| 3 | uint8_t* | ptr_inputData | Input | Input data to
encrypt or decrypt. |
| 4 | uint32_t | dataLen | Input | Length of
plain data or cipher data in bytes. |
| 5 | uint8_t* | ptr_outData | Output | Pointer to
store cipher text/plain text as output. |
| 6 | uint8_t* | ptr_nonce | Input | Pointer for
the Nonce value. |
| 7 | uint32_t | nonceLen | Input | Length of
Nonce between 7 to 13 bytes. |
| 8 | uint8_t* | ptr_authTag | Output/Input | Pointer to
store authentication tag value. Provide value while decryption
operation. |
| 9 | uint32_t | authTagLen | Input | Length of
Authentication tag between 4 to 16 bytes. |
| 10 | uint8_t* | ptr_aad | Input | Pointer for
additional authentication data. It is optional to use, so it can be
NULL also. |
| 11 | uint32_t | aadLen | Input | Length of
additional data in bytes, as it is optional so it can be 0
also. |
Returns
| Return Type | Description |
|---|
| crypto_Aead_Status_E | Function
returns the status of the API. |
Prerequisites
- To use the HW handler, the
algorithm must be enabled in Crypto v4 in MPLAB® Code Configurator.
- To use the SW handler, the
algorithm must be enabled in wolfCrypt, and linked to Crypto V4 in MPLAB® Code
Configurator.
Example
#define sessionID 1
crypto_Hash_Status_E status;
crypto_HandlerType_E handlerType_en = CRYPTO_HANDLER_SW_WOLFCRYPT;
crypto_CipherOper_E cipherOper_en = CRYPTO_CIOP_ENCRYPT;
st_Crypto_Aead_AesCcm_ctx AesCcm_ctx;
uint8_t inputData[32] = {/*data*/};
uint32_t dataLen = sizeof(inputData);
uint8_t key[32] = {/*data*/};
uint32_t keyLen = sizeof(key);
uint8_t outData[32];
uint8_t nonce[13] = {/*data*/};
uint32_t nonceLen = sizeof(nonce);
uint8_t authTag[32] = {/*data*/};
uint32_t authTagLen = 16; //tag length 4-16
uint8_t aad[32] = {/*data*/};
uint32_t aadLen = sizeof(aad);
status = Crypto_Aead_AesCcm_Init(
&AesCcm_ctx,
handlerType_en,
key,
keyLen,
sessionID
);
status = Crypto_Aead_AesCcm_Cipher(
&AesCcm_ctx,
cipherOper_en,
inputData,
dataLen,
outData,
nonce,
nonceLen,
authTag,
authTagLen,
aad,
aadLen
);