47.6.2.6.2 Normal Frequency (NFRQ)
For Normal Frequency generation, the period time (T) is controlled by the period register (PER). The waveform generation output (WO[y]) is toggled on each compare match between COUNT and CCy, and the corresponding Match or Capture Channel y Interrupt Flag (INTFLAG.MCy) will be set.
The following steps must be performed to operate the TCC in Normal Frequency (NFRQ) Waveform Generation Operations.
- Configure the clock source for the TCC Instance in the Main Clock Controller (MCLK) and enable the APB BUS clock for the TCC Instance by writing a ‘1’ to the TCCx_ bit in the APB Mask register of the MCLK (i.e. enable CLK_TCC0_APB for TCC0 by setting TCC0_ bit (APBCMASK<3>), CLK_TCC1_APB for TCC1 by setting TCC1_ bit (APBCMASK<4>) etc.).
- Enable Generic clock for TCC Instance (e.g. enable GCLK_TCC0 for TCC0 by setting PCHCTRL31.CHEN bit PCHCTRL31<6>, GCLK_TCC1 for TCC1 by setting PCHCTRL32.CHEN bit PCHCTRL32<6> etc.).
- Select desired Prescaler by setting CTRLA.PRESCALER bits (CTRLA<10:8>).
- Select matrix routing to desired port pins for generated output waveform, by configuring OTMX bits (WEXCTRL.WEXCTRL<1:0>).
- Set Waveform Generation Operations to Normal Frequency Operation (NRFQ) by clearing WAVE.WAVEGEN bits (WAVE<2:0> =0)
- Load the selected Compare/Capture (CCy) register (e.g. CC0<31:0>) with the desired compare match value. The generated output will toggle on this match.
- Load the period register PER<31:0> with the desired time period value.
- Set Counter to count in up direction by clearing CTRLBCLR.DIR bit (CTRLBCLR<0> = 1). To change the counter direction down set counter direction bit CTRLBSET.DIR(CTRLBSET<0> =1) The waveform output of a channel CCy can be inverted by configuring the corresponding Waveform Output Invert Enable bit DRVCTRL.INVENy bits where y = 0,1,2…7. For example, when the CC0 register is used for the duty cycle, the corresponding INVEN0 bit (DRVCTRL<16>) decides inversion.
- If overflow interrupt is used, set INTENSET.OVF bit (INTENSET<0>) and configure the NVIC by setting group priority, sub priority and enabling TCCx IRQ.
- Enable TCC by setting CTRLA.ENABLE bit (CTRLA<1>).
- To know how to clear interrupts, see Interrupts.