9.1.3 Register Synchronization

Overview

Most of the peripherals are composed of one digital bus interface connected to the APB or AHB bus and running from a corresponding clock in the Main Clock domain, and one peripheral core running from the peripheral Generic Clock (GCLK).

Communication between these clock domains must be synchronized. This mechanism is implemented in hardware, so the synchronization process takes place even if the peripheral generic clock is running from the same clock source and on the same frequency as the bus interface.

As shown in the following figure, each register that requires synchronization has its individual synchronizer and its individual synchronization status bit in the Synchronization Busy register (SYNCBUSY).
Note: For registers requiring read-synchronization and write-synchronization, the corresponding bit in the SYNCBUSY register is shared.

Synchronization is denoted by the "Read-Synchronized” (bits) and "Write-Synchronized” (bits) property in each individual register description.

Figure 9-1. Register Synchronization Overview

General Write Synchronization

Write-Synchronization is triggered by writing to a register in the peripheral clock domain (GCLK). The respective bit in the Synchronization Busy register (SYNCBUSY) will be set when the write-synchronization starts and cleared when the write-synchronization is complete. Refer also to Synchronization Delay.

When write-synchronization is ongoing for a register, any subsequent write attempts to this register will be discarded, and an error will be reported though the Peripheral Access Controller (PAC).

For example, the REGA, REGB are 8-bit core registers, and the REGC is a 16-bit core register.

OffsetRegister
0x00REGA
0x01REGB
0x02REGC
0x03

Synchronization is per register, therefore multiple registers can be synchronized in parallel. Consequently, after the REGA (8-bit access) was written, the REGB (8-bit access) can be written immediately without error.

The REGC (16-bit access) can be written without affecting the REGA or REGB registers. If the REGC register is written to in two consecutive 8-bit accesses without waiting for synchronization, the second write attempt will be discarded and an error is generated through the PAC.

A 32-bit access to offset 0x00 will write all three registers. The REGA, REGB, and REGC registers can be updated at different times because of independent write synchronization.

General Read Synchronization

Read-synchronized registers are synchronized each time the register value is updated but the corresponding SYNCBUSY bits are not set. Reading a read-synchronized register does not start a new synchronization, it returns the last synchronized value.

Note: The corresponding bits in SYNCBUSY will automatically be set when the device wakes up from sleep because read-synchronized registers need to be synchronized. Therefore reading a read-synchronized register before its corresponding SYNCBUSY bit is cleared will return the last synchronized value before sleep mode.

Moreover, if a register is also write-synchronized, any write access while the SYNCBUSY bit is set will be discarded and generate an error.

Completion of Synchronization

In order to check if synchronization is complete, the user can either poll the relevant bits in SYNCBUSY or use the Synchronization Ready interrupt (if available). The Synchronization Ready interrupt flag will be set when all ongoing synchronizations are complete, i.e. when all bits in SYNCBUSY are '0'.

Synchronization Delay

The synchronization will delay read and writer accesses by a certain amount. This delay D is within the range of:

5×PGCLK + 2×PAPB < D < 6×PGCLK + 3×PAPB

Where,

PGCLK is the period of the generic clock and PAPB is the period of the peripheral bus clock. A normal peripheral bus register access duration is 2×PAPB.