4 Fast Fourier Transform (FFT)
Principle
The Fast Fourier Transform (FFT) is a versatile tool for signal analysis. The general idea, in terms of electronic signals, is to de-compose a given signal (in the time domain) into sine-shaped components (in the frequency domain). Each component has a frequency, a phase, and an amplitude. The inverse operation is adding all components and will return a signal that is, in a theoretical limit, identical to the original input signal. By providing the parameters of the components, FFT can serve as a filtering tool: It can isolate a periodic signal in a noisy environment and quantify amplitudes and frequencies, detect frequency shifts of a signal, or distinguish amplitudes in high and low-frequency bands for controlling your disco lights.
Several libraries are available that implement FFT and could run on AVR devices. Here, kissFFT was chosen because it focuses on simplicity and compactness: It is easy to integrate into an AVR project, it is implemented in C, and has a useful licensing model (BSD-3-Clause). On the other hand, there are no windowing functions (aside from the implicit rectangular window when picking data blocks out of a stream) and no analysis features such as peak localization - this is up to the application. You may prefer different criteria for your library or even implement your own FFT functionality, but the general upshots from this document are also valid there.
Example
In this section, we examine the implementation and the example code we have created.
The code shows how to run FFT and measure the speed of execution. For simplicity, we use a hard-coded input signal for the FFT algorithm:
const int16_t sinewave[1024] = { ... }; - Sine wave with fundamental frequency f0 = 440 Hz
- Sampling rate fS = 44.1 kHz
- DC offset
- Strong harmonic overtones (”fuzz” effect, deliberately added)
The nfft parameter selects the sample length in
kissFFT, i.e., how many data points are used for the FFT operation. It also
determines the number of frequency bins (nfft / 2) in the
operation’s output and hence, the width of each bin
(fS/nfft). Consequently,
nfft affects the speed of the filter.
In the example, we select:
int nfft = 800;and
therefore:- Number of bins
nfft / 2 = 400 - Bin width =
2fS /
nfft≈ 110 Hz
The resulting bin width will work well with the known fundamental
frequency of 440 Hz of the example - but for speed optimization, use values
for nfft that are powers of two (e.g., 64 or
256).
kiss_fftr(cfg, cpx_in , cpx_out); // The actual FFT operation
where cfg = kiss_fftr_alloc(nfft, 0, 0, 0) is a
required set of configuration parameters, cpx_in is the
input data (real) and cpx_out is the complex output data.
cpx.
Nonetheless, the input signal is a sequence of ADC sampling values and
hence, comprises only real numbers.Now the application
can proceed and evaluate specific information in cpx_out[n]
for its purposes. In our case, we calculate the power spectrum
pwr, send it to the PC using the USART peripheral,
and plot it on the PC using the Data Visualizer:
pwr:
//Calculating the power spectrum
pwr = sqrt(cpx_out[n].r * cpx_out[n].r + cpx_out[n].i * cpx_out[n].i);For
each frequency bin n, the absolute value of the complex result vector
cpx_out[n] is calculated from its real and imaginary
components, cpx_out[n].r and cpx_out[n].i,
respectively. When the device is connected to a PC, the MPLAB® Data Visualizer can be used for signal analysis. The
following figure shows the FFT of the aforementioned input signal. The upper
plot displays the variable values, as sent by the USART: The real and the
imaginary components of cpx_out[n] share one scale. Next is
the iteration counter in yellow, followed by the power spectrum in red.
- Bin 0 is defined by the kissFFT library to contain the DC offset of the signal (clipped for legibility)
- Bin 4 contains the fundamental, around 440 Hz
- The natural
harmonics can be identified:
- 2nd harmonic at bin 8
- (There is no 3rd harmonic component at bin 12)
- 4th harmonic at bin 16
- 5th harmonic at bin 20
- The “fuzzy” look of the original signal is caused by the dominant components in bins 24 and 28, representing the sixth and seventh harmonics at around 2.65 kHz and 3.09 kHz, respectively
- Even higher harmonics and high-frequency noise components can be identified, for example, the tenth harmonic at bin 40
Performance and Properties
In comparison to other filter techniques, FFT is not easy on CPU load:
depending on nfft (and the application’s requirements), the
device’s CPU can be busy for a substantial time.
PORTD.OUTSET = PIN6_bm; // Make PD6 output logic high
kiss_fftr(cfg, cpx_in , cpx_out); // The actual FFT operation
PORTD.OUTCLR = PIN6_bm; // Make PD6 output logic low
The measured duration can be converted to ‘number of FFT per
MHz’ to compare performance or scale it with clock frequency. This method is
recommended for applications where timing and CPU load are critical.- Select “Simulator” as the connected tool in the project properties.
- Add suitable
breakpoints right before and after the function call
kiss_fftr(...);. - Find the Stopwatch window (Window → Debugging → Stopwatch).
- Run the debugger.
- When the debugger halts at a breakpoint, the Stopwatch window will display the number of virtual clock cycles used since the previous breakpoint or start and the current breakpoint.
The following table lists measured performance done on the Curiosity Nano.
| nfft | Cycles Per FFT |
|---|---|
| 4 | 5,300 |
| 8 | 12,000 |
| 16 | 30,100 |
| 32 | 67,000 |
| 64 | 161,000 |
| 128 | 348,000 |
| 256 | 810,000 |
| 512 | 1,750,000 |
As an example, an FFT with nfft=64 uses about 161 kilocycles
per FFT, corresponding to 6.2 FFT per MHz. Consequently, a device running at
a core frequency of 20 MHz could perform twenty times as many, i.e., 124 FFT
per second. If the device uses an external crystal with only 32.768 kHz, the
same FFT operation takes apporximately five seconds.
The maximum nfft value is depending on the actual memory
configuration of the device and the memory requirements of the rest of
the application.
For speed optimization, use values for nfft that are
powers of two (e.g., 64 or 256).
Conclusion and Use Cases
We have shown that an AVR device can perform Fast Fourier Transform using a third-party library (kissFFT). The FFT can provide valuable information other digital filtering techniques can’t, but at the cost of CPU cycles: It depends on the application’s requirements and details whether the FFT can be run continuously or not. Alternatively, an FFT can only occasionally be used to optimize parameters for other, faster filters.
Another point to keep in mind is the virtual precision, as suggested by the power spectrum, vs. the actual accuracy of the measurement:
One aspect is the quality of the input sample data and the time base used: The oscillator providing the time base can suffer a temperature drift of several percent. This is less of a problem for self-contained applications for signal analysis, especially when there is a short time between sampling and usage of the FFT. Though, it is relevant when interacting with external devices that have their own time base.
The other aspect is the width of a frequency bin, determined by the signal’s
sampling rate and nfft: In the example above, the power
spectrum was well suited to identify higher harmonics. On the other hand,
even when exploiting the tenth harmonic, we can not determine whether the
fundamental component was actually tuned to 440 Hz or, musically speaking,
de-tuned.