7.2 Factory Defaults
You can reset configuration of the switch on the Factory Defaults page. Only the IP configuration is retained. The new configuration is available immediately, which means that restart is not necessary.

Note: Restoring factory default can also be performed by making a physical loopback between port 1 and port 2 within the first minute from switch reboot. In the first minute after boot, 'loopback' packets will be transmitted at port 1. If a 'loopback' packet is received at port 2 the switch will do a restore to default.