4.2.3.1 diag_result_t

enum diag_result_t

Contains return codes for the diagnostic tests.

DIAG_PASS

0x81U - Indicates that no Fault was detected by the diagnostic

DIAG_FAIL

0x42U - Indicates that a Fault was detected by the diagnostic

DIAG_INVALID_ARG

0x24U - Indicates that the diagnostic was unsuccessful due to one or more invalid input arguments when calling the function

DIAG_UNDEFINED

0x7EU - Indicates that the result of the diagnostic is undefined due to incorrect usage of the API

DIAG_NVM_STORE_ERROR

0xBDU - Indicates that the Nonvolatile Memory (NVM) controller reported an error when attempting to write a value to nonvolatile memory

DIAG_NOT_EXECUTED

0x18U - Indicates that the test was not executed for the current run

Note:

The enum values are chosen with a specific bit pattern to not overlap with the March diagnostic data backgrounds and avoid accidentally reporting an incorrect result.