2 Building AT91Bootstrap Project Using MPLABx

  • Open a console and execute the following command to clone at91bootstrap repository into a directory named at91bootstrap.X
    git clone https://github.com/linux4sam/at91bootstrap at91bootstrap.X
  • Open at91bootstrap.X directory as project in MPLABx

Configure Compiler

  • Open project properties window, and choose “Makefile” option to configure the compiler:
  • Default option is configured to use ARM gcc. To use xc32, replace all instances of arm-none-eabi- to xc32- as follows
Note: For the build to be successful, the configured compiler should be available in the system path.

Configure Target

  • Open project properties window, and choose “Kconfig” option to configure the build target:
  • Click on “LOAD” button and navigate to the configs folder inside at91bootstrap.X directory. You need to choose the default configuration file (defconfig) based on what you need the at91boostrap to do

    Debug/Run application from within MPLABx

    • Load {Curiosity_kit}_bkpt_none_defconfig. For example, on SAM9X75 Curiosity Board, select sam9x75eb_bkptnone_defconfig as the configuration file
    • Click on “Apply” and “OK” buttons to configure the project
    • You can see that the MPU product is now selected as “SAM9X7” and the primary operation is selected as “Configure and Stop”

    Load and Run application from an SD card

    • Load {Curiosity_kit}sd_uboot_defconfig. For example, on SAM9X75 Curiosity Kit, select sam9x75ebsd_uboot_defconfig as the configuration file
    • Click on “Apply” and “OK” buttons to configure the project
    • You can see that the MPU product is now selected as “SAM9X7” and the primary operation is selected as “Load and launch next software”
    • Edit the Option “Next Software Image File Name” from u-boot.bin to harmony.bin

Build Target

Once the target configuration is applied in the properties window, you can build the at91boostrap just like any other MPLABx project. After the build is complete, you can find the generated binary files under build/binaries directory.