5.5.2.1 .align algn[, fill[, max-skip]]
Pad the location counter (in the current subsection) to a particular storage boundary.
algn is the address alignment required.
The location counter is advanced until it is a multiple of the requested alignment. If the
location counter is already a multiple of the requested alignment, no change is needed or
made. For dsPIC33A, an alignment of 4 is
required. The requested alignment must be a power of 2.
fill is optional. If not specified:
- In a data section, a value of
0x00is used to fill the skipped bytes. - In a code section, the last specified
.fillvalueis used to fill the skipped bytes.
max-skip is optional. If specified, it
is the maximum number of bytes that should be skipped by this directive. If doing the
alignment would require skipping more bytes than the specified maximum, then the alignment
is not done at all.
Alignment within a section is required for modulo addressing. It is worth
noting that the overall section alignment reflects the greatest alignment of any
.align directives that are included. Further, the assembler must pad
out the section length to match its alignment. This is done in order to preserve the
requested alignment in case the section is combined with other sections of the same name
during the link. To avoid unnecessary padding of aligned sections, use the section name *,
which identifies a unique section that will never be combined.