2.1 Programming the Wi-Fi® Module and Enabling HUT Mode
Perform the following steps to program the WILCS02 Module and enable the HUT mode.
- Download the combined (HUT + Mission mode) firmware image from the product webpage WILCS02UE.
- Make connections between the Wi-Fi module on the application board and Test PC as illustrated in the following figure to perform DFU. Program the combined (HUT + Mission mode) firmware image using DFU. For more details on the DFU process, refer to the Device Firmware Update (DFU) section of the WILCS02 Application
Developer’s Guide.
Figure 2-1. DFU Setup - Restart the module; it will automatically boot in the HUT mode.