51.12.35 SDMMC Capabilities 1 Register
Instance | Reset Value |
---|---|
SDMMC0 | 0x00200F77 |
SDMMC1 | 0x00200070 |
Name: | SDMMC_CA1R |
Offset: | 0x44 |
Property: | Read/Write |
Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
Access | |||||||||
Reset |
Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
CLKMULT[7:0] | |||||||||
Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W | |
Reset |
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
RTMOD[1:0] | TSDR50 | TCNTRT[3:0] | |||||||
Access | R/W | R/W | R/W | R/W | R/W | R/W | R/W | ||
Reset |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
DRVDSUP | DRVCSUP | DRVASUP | DDR50SUP | SDR104SUP | SDR50SUP | ||||
Access | R/W | R/W | R/W | R/W | R/W | R/W | |||
Reset |
Bits 23:16 – CLKMULT[7:0] Clock Multiplier
This field indicates the multiplier factor between the Base Clock (BASECLK) used for the Divided Clock Mode and the Multiplied Clock (MULTCLK) used for the Programmable Clock mode (see SDMMC_CCR).
Reading this field to 0 means that the Programmable Clock mode is not supported.
Bits 15:14 – RTMOD[1:0] Retuning Modes
This field selects the retuning method and limits the maximum data length.
There are two retuning timings: Retuning Request (RTREQ) controlled by the SDMMC, and expiration of a Retuning timer controlled by the user. By receiving either timing, the user executes the retuning procedure just before a next command issue.
The maximum data length per read/write command is restricted so that retuning procedures can be inserted during data transfers.
Retuning Mode 1:
The SDMMC does not have any internal logic to detect when retuning needs to be performed. In this case, the user should maintain all retuning timings by using the Retuning Timer. To enable inserting the retuning procedure during data transfers, the data length per Read/Write command must be limited to 4 Mbytes.
Retuning Mode 2:
The SDMMC has the capability to indicate the retuning timing by Retuning Request (RTREQ) during data transfers. Then the data length per Read/Write command must be limited to 4 Mbytes.
During nondata transfer, retuning timing is determined by either Retuning Request or Retuning Timer. If Retuning Request is used, Retuning Timer should be disabled.
Retuning Mode 3:
The SDMMC has the capability to take care of the retuning during data transfer (Auto Retuning). Retuning Request is not generated during data transfers and there is no limitation to data length per Read/Write command.
During nondata transfer, retuning timing is determined either by Retuning Request or Retuning Timer. If Retuning Request is used, Retuning Timer should be disabled.
Value | Name | Description | Data Length |
---|---|---|---|
0 | MODE1 | Timer | 4 Mbytes (Max) |
1 | MODE2 | Timer and Retuning Request | 4 Mbytes (Max) |
2 | MODE3 | Auto Retuning (for transfer) Timer and Retuning Request | Any |
3 | – | Reserved | – |
Bit 13 – TSDR50 Use Tuning for SDR50
If this bit is set to 1, the SDMMC requires tuning to operate SDR50 (tuning is always required to operate SDR104).
Value | Description |
---|---|
0 |
SDR50 does not require tuning. |
1 |
SDR50 requires tuning. |
Bits 11:8 – TCNTRT[3:0] Timer Count For Retuning
This field indicates an initial value of the Retuning Timer for Retuning Mode (RTMOD) 1 to 3. Reading this field at 0 means that the Retuning Timer is disabled. The Retuning Timer initial value ranges from 0 to 1024 seconds.
tTIMER = 2(TCNTRT – 1)Seconds
Bit 6 – DRVDSUP Driver Type D Support
Value | Description |
---|---|
0 | Driver type D is not supported. |
1 | Driver type D is supported. |
Bit 5 – DRVCSUP Driver Type C Support
Value | Description |
---|---|
0 | Driver type C is not supported. |
1 | Driver type C is supported. |
Bit 4 – DRVASUP Driver Type A Support
Value | Description |
---|---|
0 | Driver type A is not supported. |
1 | Driver type A is supported. |
Bit 2 – DDR50SUP DDR50 Support
Value | Description |
---|---|
0 | DDR50 mode is not supported. |
1 | DDR50 mode is supported. |
Bit 1 – SDR104SUP SDR104 Support
Value | Description |
---|---|
0 | SDR104 mode is not supported. |
1 | SDR104 mode is supported. |
Bit 0 – SDR50SUP SDR50 Support
Value | Description |
---|---|
0 | SDR50 mode is not supported. |
1 | SDR50 mode is supported. |