1.3.2 Net System Service Usage

Description

The NET System Service provides simple APIs to enable Server or Client Connectivity for either TCP or UDP. The User need not take care of intermediate states of a TCPIP Connection, as the Service internally takes care of that. User is not required to have Security domain knowledge to establish a secured connection via the application using NET System Service library.

Command Line:

User can follow below commands for NET System Service:

  1. sysnethelp

    NET System Service help command which displays the supported CLI commands

    resized_sysnethelp_cli
  2. sysnet open

    Command for Reconfiguring an already open instance of Net System Service

    sysnetopen_cli
  3. sysnet close

    Command to close the instance of Net System Service

    sysnetclose_cli
  4. sysnet send

    Command to send message on the network connection established by the instance of Net System Service

    sysnetsend_cli
  5. sysnet get info

    Command for knowing the Current Information for all the Instances of Net System Service

    sysnetgetinfo_cli

Abstraction Model

The NET System Service library provides an abstraction to the NetPres/ TCPIP APIs to provide following functionalities.

  • Connectivity for TCP Client

  • Connectivity for TCP Server

  • Connectivity for UDP Client

  • Connectivity for UDP Server

  • Self Healing

  • Reduce code user has to write

  • Reduce time to develop and maintain

The following diagram depicts the Net System Service abstraction model.

NetService_abstract

How The Library Works

By default MHC generated code provides all the functionalities to enable Client or Server mode applicatation, with TCP or UDP as the IP Protocol. User needs to configure the required Client or Server mode configuration using MHC. User needs to call the SYS_NET_Open() API with a valid callback to open an instance of the Client/ Server configured in the MHC.

NetOpen

The User Application is expected to call SYS_NET_Task() API periodically as this API ensures that the Net System service is able to execute its state machine to process any messages and invoke the user callback for any events.

NetTask

The User Application can call SYS_NET_CtrlMsg() API in case it wants to disconnect the opened connection or to reconnect using different configuration.

NetCtrlMsg