28.6.12 Events
The ADC can generate the following output
events:
- Result Ready (RESRDY): Generated when the conversion is complete and the result is available.
- Window Monitor (WINMON): Generated when the window monitor condition match.
Setting an Event Output bit in the Event Control Register (EVCTRL.xxEO=1) enables the corresponding output event. Clearing this bit disables the corresponding output event. Refer to the Event System chapter for details on configuring the event system.
The peripheral can take the following
actions on an input event:
- Start conversion (START): Start a conversion.
- Conversion flush (FLUSH): Flush the conversion.
Setting an Event Input bit in the Event Control register (EVCTRL.xxEI=1) enables the corresponding action on input event. Clearing this bit disables the corresponding action on input event.
Note: If several events are connected to the
ADC, the enabled action will be taken on any of the incoming events. The events must be
correctly routed in the Event System.