1.11 I2C Driver Synchronous - Multi Client

This example application demonstrates the multi-client feature of the synchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor.

Description

This example uses the I2C driver in asynchronous mode and demonstrates the multi-client feature. The example uses a IO1 Xplained Pro Extension Kit that has a temperature sensor and an EEPROM, both interfaced on the same I2C bus.

Two application tasks are created which act as clients to the same instance of the I2C driver:

APP_I2C_TEMP_SENSOR_Tasks:

Reads temperature every 1 second, prints on console and notifies the EEPROM client. The Time System Service is used to generate a callback every 1 second

APP_I2C_EEPROM_Tasks:

Writes temperature values to the EEPROM once the temperature read complete notification is received. The task also reads and prints the last five saved temperature data from the EEPROM when user enters any key on the console.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/i2c/sync/i2c_multi_slave/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_c21n_xpro_freertos.XMPLABX project for SAMC21N Xplained Pro Evaluation Kit

Running the Application

  1. Connect a micro USB cable to the DEBUG port.
  2. Open the Terminal application (Ex.:Tera term) on the computer.
  3. Configure the DEBUG port settings as follows:
    • Baud : 115200
    • Data : 8 Bits
    • Parity : None
    • Stop : 1 Bit
    • Flow Control : None
  4. Build and program the application using the MPLAB X IDE.
  5. Observe the temperature values getting printed on the terminal application every 1 second and temperature value written into EEPROM notification as shown below:
  6. Press any key on the terminal, last 5 temperature values will be read from the EEPROM and displayed as shown below: