1 Building and Installing the GNU Tool Chain
This chapter shows how to build and install, from source code, a complete development environment for the AVR processors using the GNU toolset. There are two main sections, one for Linux, FreeBSD, and other Unix-like operating systems, and another section for Windows.
Building and Installing under Linux, FreeBSD, and Others
The default behaviour for most of these
tools is to install every thing under the
/usr/local directory.
In order to keep the AVR tools separate from the
base system, it is usually better to install
everything into /usr/local/avr.
If the /usr/local/avr directory
does not exist, you should create it before
trying to install anything. You will need
root access to install
there. If you don't have root access to the
system, you can alternatively install in your
home directory, for example, in
$HOME/local/avr. Where
you install is a completely arbitrary decision,
but should be consistent for all the tools.
You specify the installation directory
by using the --prefix=dir
option with the configure
script. It is important to install all the AVR
tools in the same directory or some of the tools
will not work correctly. To ensure consistency
and simplify the discussion, we will use
$PREFIX to refer to
whatever directory you wish to install in. You
can set this as an environment variable if you
wish as such (using a Bourne-like shell):
$ PREFIX=$HOME/local/avr $ export PREFIX
Be sure that you have
your PATH environment
variable set to search the directory you
install everything in before you
start installing anything. For example,
if you use
--prefix=$PREFIX, you
must have $PREFIX/bin
in your exported PATH.
As such:
$ PATH=$PATH:$PREFIX/bin $ export PATH
If you have
CC set to anything
other than avr-gcc in
your environment, this will cause the
configure script to fail. It is best to
not have CC set at
all.
It is usually the best to use the latest released version of each of the tools.
Required Tools
-
GNU Binutils http://sources.redhat.com/binutils/ Installation
Optional Tools
You can develop programs for AVR devices without the following tools. They may or may not be of use for you.
GNU Binutils for the AVR target
The binutils
package provides all the low-level utilities
needed in building and manipulating object
files. Once installed, your environment will
have an AVR assembler (avr-as),
linker (avr-ld), and librarian
(avr-ar and
avr-ranlib). In
addition, you get tools which extract data from
object files (avr-objcopy),
dissassemble object file information
(avr-objdump), and
strip information from object files
(avr-strip). Before we
can build the C compiler, these tools need to be
in place.
Download and unpack the source files:
Replace
<version> with
the version of the package you
downloaded.
If you obtained a gzip
compressed file (.gz), use
gunzip instead of
bunzip2.
binutils in a
subdirectory so as not to pollute the source
with the compiled files. This is recommended by
the binutils
developers.The next step is to configure and build
the tools. This is done by supplying arguments
to the configure script that
enable the AVR-specific options.
If you don't specify the
--prefix option, the
tools will get installed in the
/usr/local hierarchy
(i.e. the binaries will get installed in
/usr/local/bin, the
info pages get installed in
/usr/local/info, etc.)
Since these tools are changing frequently, It is
preferrable to put them in a location that is
easily removed.
When configure is run,
it generates a lot of messages while it
determines what is available on your operating
system. When it finishes, it will have created
several Makefiles that are
custom tailored to your platform. At this point,
you can build the project.
BSD users should note
that the project's
Makefile uses GNU
make syntax. This means
FreeBSD users may need to build the
tools by using
gmake.
root access to
install them. To install:You should now have the programs from
binutils installed into
$PREFIX/bin. Don't
forget to set your PATH
environment variable before going to build
avr-gcc.
GCC for the AVR target
You must install avr-binutils and make sure your path is set properly before installing avr-gcc.
avr-gcc are essentially
same as for binutils:To save your self some download time,
you can alternatively download only the
gcc-core-<version>.tar.bz2
and
gcc-c++-<version>.tar.bz2
parts of the gcc. Also, if you don't need C++
support, you only need the core part and should
only enable the C language support. (Starting
with GCC 4.7 releases, these split files are no
longer available though.)
Early versions of these tools did not support C++.
The stdc++ libs are not included with C++ for AVR due to the size limitations of the devices.
AVR LibC
You must install avr-binutils, avr-gcc and make sure your path is set properly before installing avr-libc.
If you have obtained the
latest avr-libc from cvs, you will have
to run the bootstrap
script before using either of the build
methods described below.
Optionally, generation of debug information can be requested with:
where DEBUG_INFO can be
one of stabs,
dwarf-2, or
dwarf-4.
The default is to not generate any debug information, which is suitable for binary distributions of avr-libc, where the user does not have the source code installed the debug information would refer to.
AVRDUDE
It has been ported to windows (via MinGW or cygwin), Linux and Solaris. Other Unix systems should be trivial to port to.
avrdude is part of the
FreeBSD ports system. To install it, simply do
the following:Installation into the
default location usually requires root
permissions. However, running the
program only requires access permissions
to the appropriate
ppi(4) device.
configure
system, as such:GDB for the AVR target
GDB also uses the
configure system, so to
build and install:
SimulAVR
SimulAVR also uses the
configure system, so to
build and install:
You might want to have already installed avr-binutils, avr-gcc and avr-libc if you want to have the test programs built in the simulavr source.
AVaRICE
These install notes are not applicable to avarice-1.5 or older. You probably don't want to use anything that old anyways since there have been many improvements and bug fixes since the 1.5 release.
configure system, so to
build and install:AVaRICE uses the BFD
library for accessing various binary
file formats. You may need to tell the
configure script where to find the lib
and headers for the link to work. This
is usually done by invoking the
configure script like this (Replace
<hdr_path> with
the path to the bfd.h
file on your system. Replace
<lib_path> with
the path to libbfd.a on
your system.):
$ CPPFLAGS=-I<hdr_path> LDFLAGS=-L<lib_path> ../configure --prefix=$PREFIX
Building and Installing under Windows
Building and installing the toolchain under Windows requires more effort because all of the tools required for building, and the programs themselves, are mainly designed for running under a POSIX environment such as Unix and Linux. Windows does not natively provide such an environment.
There are two projects available that provide such an environment, Cygwin and MinGW. There are advantages and disadvantages to both. Cygwin provides a very complete POSIX environment that allows one to build many Linux based tools from source with very little or no source modifications. However, POSIX functionality is provided in the form of a DLL that is linked to the application. This DLL has to be redistributed with your application and there are issues if the Cygwin DLL already exists on the installation system and different versions of the DLL. On the other hand, MinGW can compile code as native Win32 applications. However, this means that programs designed for Unix and Linux (i.e. that use POSIX functionality) will not compile as MinGW does not provide that POSIX layer for you. Therefore most programs that compile on both types of host systems, usually must provide some sort of abstraction layer to allow an application to be built cross-platform.
MinGW does provide somewhat of a POSIX
environment, called MSYS, that allows you to
build Unix and Linux applications as they woud
normally do, with a configure
step and a make step. Cygwin
also provides such an environment. This means
that building the AVR toolchain is very similar
to how it is built in Linux, described above.
The main differences are in what the PATH
environment variable gets set to, pathname
differences, and the tools that are required to
build the projects under Windows. We'll take a
look at the tools next.
Tools Required for Building the Toolchain for Windows
These are the tools that are currently used to build an AVR tool chain. This list may change, either the version of the tools, or the tools themselves, as improvements are made.
-
MinGW Download the MinGW Automated Installer, 20100909 (or later) <http://sourceforge.net/projects/mingw/files/Automated%20MinGW%20Installer/mingw-get-inst/mingw-get-inst-20100909/mingw-get-inst-20100909.exe/download>
-
Run mingw-get-inst-20100909.exe
-
In the installation wizard, keep the default values and press the "Next" button for all installer pages except for the pages explicitly listed below.
-
In the installer page "Repository Catalogues", select the "Download latest repository catalogues" radio button, and press the "Next" button
-
In the installer page "License Agreement", select the "I accept the agreement" radio button, and press the "Next" button
-
In the installer page "Select Components", be sure to select these items:
-
C compiler (default checked)
-
C++ compiler
-
Ada compiler
-
MinGW Developer Toolkit (which includes "MSYS Basic System").
-
-
Install.
-
-
Install Cygwin
-
Install everything, all users, UNIX line endings. This will take a *long* time. A fat internet pipe is highly recommended. It is also recommended that you download all to a directory first, and then install from that directory to your machine.
-
GMP, MPFR, and MPC are required to build GCC.
GMP is a prequisite for building MPFR. Build GMP first.
MPFR is a prerequisite for building MPC. Build MPFR second.
-
Build GMP for MinGW
-
Latest Version
-
Build script:
./configure 2>&1 | tee gmp-configure.log make 2>&1 | tee gmp-make.log make check 2>&1 | tee gmp-make-check.log make install 2>&1 | tee gmp-make-install.log -
GMP headers will be installed under /usr/local/include and library installed under /usr/local/lib.
-
-
Build MPFR for MinGW
-
Latest Version
-
Build script:
./configure --with-gmp=/usr/local --disable-shared 2>&1 | tee mpfr-configure.log make 2>&1 | tee mpfr-make.log make check 2>&1 | tee mpfr-make-check.log make install 2>&1 | tee mpfr-make-install.log -
MPFR headers will be installed under /usr/local/include and library installed under /usr/local/lib.
-
-
Build MPC for MinGW
-
Latest Version
-
Build script:
./configure --with-gmp=/usr/local --with-mpfr=/usr/local --disable-shared 2>&1 | tee mpfr-configure.log make 2>&1 | tee mpfr-make.log make check 2>&1 | tee mpfr-make-check.log make install 2>&1 | tee mpfr-make-install.log -
MPFR headers will be installed under /usr/local/include and library installed under /usr/local/lib.
-
-
Install Doxygen
-
Version 1.7.2
-
Download and install.
-
-
Install NetPBM
-
Version 10.27.0
-
From the GNUWin32 project: <http://gnuwin32.sourceforge.net/packages.html>
-
Download and install.
-
-
Install fig2dev
-
Version 3.2 patchlevel 5c
-
From WinFig 4.62: <http://www.schmidt-web-berlin.de/winfig/>
-
Download the zip file version of WinFig
-
Unzip the download file and install fig2dev.exe in a location of your choice, somewhere in the PATH.
-
You may have to unzip and install related DLL files for fig2dev. In the version above, you have to install QtCore4.dll and QtGui4.dll.
-
-
Install MiKTeX
-
Version 2.9
-
Download and install.
-
-
Install Ghostscript
-
Version 9.00
-
Download and install.
-
In the \bin subdirectory of the installaion, copy gswin32c.exe to gs.exe.
-
-
Set the TEMP and TMP environment variables to c:\temp or to the short filename version. This helps to avoid NTVDM errors during building.
Building the Toolchain for Windows
All directories in the PATH enviornment variable should be specified using their short filename (8.3) version. This will also help to avoid NTVDM errors during building. These short filenames can be specific to each machine.
Build the tools below in MinGW/MSYS.
-
Binutils
-
Open source code pacakge and patch as necessary.
-
Configure and build in a directory outside of the source code tree.
-
Set PATH, in order:
-
<MikTex executables>
-
<ghostscript executables>
-
/usr/local/bin
-
/usr/bin
-
/bin
-
/mingw/bin
-
c:/cygwin/bin
-
<install directory>/bin
-
-
Configure
CFLAGS=-D__USE_MINGW_ACCESS \ ../$archivedir/configure \ --prefix=$installdir \ --target=avr \ --disable-nls \ --enable-doc \ --datadir=$installdir/doc/binutils \ --with-gmp=/usr/local \ --with-mpfr=/usr/local \ 2>&1 | tee binutils-configure.log -
Make
make all html install install-html 2>&1 | tee binutils-make.log -
Manually change documentation location.
-
-
GCC
-
Open source code pacakge and patch as necessary.
-
Configure and build in a directory outside of the source code tree.
-
Set PATH, in order:
-
<MikTex executables>
-
<ghostscript executables>
-
/usr/local/bin
-
/usr/bin
-
/bin
-
/mingw/bin
-
c:/cygwin/bin
-
<install directory>/bin
-
-
Configure
LDFLAGS='-L /usr/local/lib -R /usr/local/lib' \ CFLAGS='-D__USE_MINGW_ACCESS' \ ../gcc-$version/configure \ --with-gmp=/usr/local \ --with-mpfr=/usr/local \ --with-mpc=/usr/local \ --prefix=$installdir \ --target=$target \ --enable-languages=c,c++ \ --with-dwarf2 \ --enable-doc \ --with-docdir=$installdir/doc/$project \ --disable-shared \ --disable-libada \ --disable-libssp \ 2>&1 | tee $project-configure.log
-
Make
make all html install 2>&1 | tee $package-make.log
-
-
avr-libc
-
Open source code package.
-
Configure and build at the top of the source code tree.
-
Set PATH, in order:
-
/usr/local/bin
-
/mingw/bin
-
/bin
-
<MikTex executables>
-
<install directory>/bin
-
<Doxygen executables>
-
<NetPBM executables>
-
<fig2dev executable>
-
<Ghostscript executables>
-
c:/cygwin/bin
-
-
Configure
./configure \ --host=avr \ --prefix=$installdir \ --enable-doc \ --disable-versioned-doc \ --enable-html-doc \ --enable-xml-doc \ --enable-pdf-doc \ --enable-man-doc \ --mandir=$installdir/man \ --datadir=$installdir \ 2>&1 | tee $package-configure.log -
Make
make all install 2>&1 | tee $package-make.log -
Manually change location of man page documentation.
-
Move the examples to the top level of the install tree.
-
Convert line endings in examples to Windows line endings.
-
Convert line endings in header files to Windows line endings.
-
-
AVRDUDE
-
Open source code package.
-
Configure and build at the top of the source code tree.
-
Set PATH, in order:
-
<MikTex executables>
-
/usr/local/bin
-
/usr/bin
-
/bin
-
/mingw/bin
-
c:/cygwin/bin
-
<install directory>/bin
-
-
Set location of LibUSB headers and libraries
export CPPFLAGS="-I../../libusb-win32-device-bin-$libusb_version/include" export CFLAGS="-I../../libusb-win32-device-bin-$libusb_version/include" export LDFLAGS="-L../../libusb-win32-device-bin-$libusb_version/lib/gcc" -
Configure
./configure \ --prefix=$installdir \ --datadir=$installdir \ --sysconfdir=$installdir/bin \ --enable-doc \ --disable-versioned-doc \ 2>&1 | tee $package-configure.log -
Make
make -k all install 2>&1 | tee $package-make.log -
Convert line endings in avrdude config file to Windows line endings.
-
Delete backup copy of avrdude config file in install directory if exists.
-
-
Insight/GDB
-
Open source code pacakge and patch as necessary.
-
Configure and build in a directory outside of the source code tree.
-
Set PATH, in order:
-
<MikTex executables>
-
/usr/local/bin
-
/usr/bin
-
/bin
-
/mingw/bin
-
c:/cygwin/bin
-
<install directory>/bin
-
-
Configure
CFLAGS=-D__USE_MINGW_ACCESS \ LDFLAGS='-static' \ ../$archivedir/configure \ --prefix=$installdir \ --target=avr \ --with-gmp=/usr/local \ --with-mpfr=/usr/local \ --enable-doc \ 2>&1 | tee insight-configure.log -
Make
make all install 2>&1 | tee $package-make.log
-
-
SRecord
-
Open source code package.
-
Configure and build at the top of the source code tree.
-
Set PATH, in order:
-
<MikTex executables>
-
/usr/local/bin
-
/usr/bin
-
/bin
-
/mingw/bin
-
c:/cygwin/bin
-
<install directory>/bin
-
-
Configure
./configure \ --prefix=$installdir \ --infodir=$installdir/info \ --mandir=$installdir/man \ 2>&1 | tee $package-configure.log -
Make
make all install 2>&1 | tee $package-make.log
-
Build the tools below in Cygwin.
-
AVaRICE
-
Open source code package.
-
Configure and build in a directory outside of the source code tree.
-
Set PATH, in order:
-
<MikTex executables>
-
/usr/local/bin
-
/usr/bin
-
/bin
-
<install directory>/bin
-
-
Set location of LibUSB headers and libraries
export CPPFLAGS=-I$startdir/libusb-win32-device-bin-$libusb_version/include export CFLAGS=-I$startdir/libusb-win32-device-bin-$libusb_version/include export LDFLAGS="-static -L$startdir/libusb-win32-device-bin-$libusb_version/lib/gcc " -
Configure
../$archivedir/configure \ --prefix=$installdir \ --datadir=$installdir/doc \ --mandir=$installdir/man \ --infodir=$installdir/info \ 2>&1 | tee avarice-configure.log -
Make
make all install 2>&1 | tee avarice-make.log
-
-
SimulAVR
-
Open source code package.
-
Configure and build in a directory outside of the source code tree.
-
Set PATH, in order:
-
<MikTex executables>
-
/usr/local/bin
-
/usr/bin
-
/bin
-
<install directory>/bin
-
-
Configure
export LDFLAGS="-static" ../$archivedir/configure \ --prefix=$installdir \ --datadir=$installdir \ --disable-tests \ --disable-versioned-doc \ 2>&1 | tee simulavr-configure.log -
Make
make -k all install 2>&1 | tee simulavr-make.log make pdf install-pdf 2>&1 | tee simulavr-pdf-make.log
-