35.5.9.4 Guard Ring Outputs

Figure 35-14 shows a typical guard ring circuit. CGUARD represents the capacitance of the guard ring trace placed on the PCB. The user selects values for RA and RB that will create a voltage profile on CGUARD, which will match the selected acquisition channel.

The purpose of the guard ring is to generate a signal in phase with the CVD sensing signal to minimize the effects of the parasitic capacitance on sensing electrodes. It also can be used as a mutual drive for mutual capacitive sensing. For more information about active guard and mutual drive, refer to Microchip Application Note AN1478, “mTouch™ Sensing Solution Acquisition Methods Capacitive Voltage Divider”, available at the corporate website (www.microchip.com).

The ADC has two guard ring drive outputs, ADGRDA and ADGRDB. These outputs are routed through PPS controls to I/O pins. Refer to the “Peripheral Pin Select (PPS) Module” chapter for more details. The polarity of these outputs is controlled by the GPOL and IPEN bits.

At the start of the first precharge stage, both outputs are set to match the GPOL bit. Once the acquisition stage begins, ADGRDA changes polarity, while ADGRDB remains unchanged. When performing a double sample conversion, setting the IPEN bit causes both guard ring outputs to transition to the opposite polarity of GPOL at the start of the second precharge stage, and ADGRDA toggles again for the second acquisition. For more information on the timing of the guard ring output, refer to Figure 35-15.

Figure 35-14. Guard Ring Circuit
Figure 35-15. Differential CVD with Guard Ring Output Waveform