2.4.4.1 com_adapter_result_t
enum com_adapter_result_t
Contains codes for the return values of the bootloader communication adapter layer APIs.
COM_PASS |
0xE7U - com_adapter operation succeeded |
COM_FAIL |
0xC3U - com_adapter operation failed |
COM_INVALID_ARG |
0x96U - com_adapter operation has an invalid argument |
COM_BUFFER_ERROR |
0x69U - com_adapter operation has encountered an overflow |
COM_BUSY |
0x18U - com_adapter operation is not finished yet |
COM_TRANSPORT_FAILURE |
0x3CU - com_adapter operation is not finished yet |
COM_SEND_COMPLETE |
0x7EU - com_adapter sending operation is finished |