3 Launching the Pre-Installed Webserver Application
(Ask a Question)To launch the pre-installed Webserver application, perform the following steps:
- Connect an Ethernet cable to J2 and connect it to the same router as your PC.
- Using Linux console as the command-line interface, change to the webserver directory.
$ cd /opt/microchip/iiohttpserver - Find the IP address of the icicle kit by running.
$ ifconfig - Launch the web server by running the script.
$ ./run.sh - The webserver will now start running.
- Browse to the IP address of the Icicle kit from your host machine to view the webpage.
Important: Click MPFS Icicle Kit User Guide to update your PolarFire SoC Icicle kit to the latest binaries.