2.1 Wi-Fi Gain Table Format
The format of the Wi-Fi gain table displays below. This table needs to be filled with DG, PA and PPA values, which are unique for a given Wi-Fi channel and data rate. Microchip recommends using the default gain table and editing the gain values based on the user requirement. The default gain table can be accessed from the location mentioned in Section 7 (Gain Values Download) of the ATWINC15x0/ATWINC3400 − Integrated Serial Flash and Memory Download Procedure Application Note (DS00002378).
The following table format is an example for the DG table.
| Data Rate | Channel | |||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 | 11 | 12 | 13 | 14 | |
| WiFi_Gain_1: | ||||||||||||||
| WiFi_Gain_2: | ||||||||||||||
| WiFi_Gain_5.5: | ||||||||||||||
| WiFi_Gain_11: | ||||||||||||||
| WiFi_Gain_6: | ||||||||||||||
| WiFi_Gain_9: | ||||||||||||||
| WiFi_Gain_12: | ||||||||||||||
| WiFi_Gain_18: | ||||||||||||||
| WiFi_Gain_24: | ||||||||||||||
| WiFi_Gain_36: | ||||||||||||||
| WiFi_Gain_48: | ||||||||||||||
| WiFi_Gain_54: | ||||||||||||||
| WiFi_Gain_MCS0: | ||||||||||||||
| WiFi_Gain_MCS1: | ||||||||||||||
| WiFi_Gain_MCS2: | ||||||||||||||
| WiFi_Gain_MCS3: | ||||||||||||||
| WiFi_Gain_MCS4: | ||||||||||||||
| WiFi_Gain_MCS5: | ||||||||||||||
| WiFi_Gain_MCS6: | ||||||||||||||
| WiFi_Gain_MCS7: | ||||||||||||||
The first row represents the Wi-Fi channel number and the first column represents the data rate. The Digital Gain (DG) value has to be determined by the user for all of the combinations of the Wi-Fi channel number and data rate.
The following table format is an example for the PA and PPA gain table.
| Data Rate | Channel | |||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 | 11 | 12 | 13 | 14 | |
| WiFi_PA_1: | ||||||||||||||
| WiFi_PA_2: | ||||||||||||||
| WiFi_PA_5.5: | ||||||||||||||
| WiFi_PA_11: | ||||||||||||||
| WiFi_PA_6: | ||||||||||||||
| WiFi_PA_9: | ||||||||||||||
| WiFi_PA_12: | ||||||||||||||
| WiFi_PA_18: | ||||||||||||||
| WiFi_PA_24: | ||||||||||||||
| WiFi_PA_36: | ||||||||||||||
| WiFi_PA_48: | ||||||||||||||
| WiFi_PA_54: | ||||||||||||||
| WiFi_PA_MCS0: | ||||||||||||||
| WiFi_PA_MCS1: | ||||||||||||||
| WiFi_PA_MCS2: | ||||||||||||||
| WiFi_PA_MCS3: | ||||||||||||||
| WiFi_PA_MCS4: | ||||||||||||||
| WiFi_PA_MCS5: | ||||||||||||||
| WiFi_PA_MCS6: | ||||||||||||||
| WiFi_PA_MCS7: | ||||||||||||||
| WiFi_PPA_1: | ||||||||||||||
| WiFi_PPA_2: | ||||||||||||||
| WiFi_PPA_5.5: | ||||||||||||||
| WiFi_PPA_11: | ||||||||||||||
| WiFi_PPA_6: | ||||||||||||||
| WiFi_PPA_9: | ||||||||||||||
| WiFi_PPA_12: | ||||||||||||||
| WiFi_PPA_18: | ||||||||||||||
| WiFi_PPA_24: | ||||||||||||||
| WiFi_PPA_36: | ||||||||||||||
| WiFi_PPA_48: | ||||||||||||||
| WiFi_PPA_54: | ||||||||||||||
| WiFi_PPA_MCS0: | ||||||||||||||
| WiFi_PPA_MCS1: | ||||||||||||||
| WiFi_PPA_MCS2: | ||||||||||||||
| WiFi_PPA_MCS3: | ||||||||||||||
| WiFi_PPA_MCS4: | ||||||||||||||
| WiFi_PPA_MCS5: | ||||||||||||||
| WiFi_PPA_MCS6: | ||||||||||||||
| WiFi_PPA_MCS7: | ||||||||||||||