6 Cryptographic Algorithm Specifications
The following describes the controlling documents for the cryptographic algorithms implemented within the TA100 device.
The following describes the controlling documents for the cryptographic algorithms implemented within the TA100 device.
The TA100 device calculates cryptographic digests using
SHA-256:
HMAC calculations are performed with key sizes varying from 16 to 64 bytes. The
underlying algorithm is always SHA-256.
Authorization session establishment uses the HMAC/SHA-256 - counter key derivation
function specified in the following document. This KDF is also supported by the
KDF command for general purpose use:Symmetric encryption implemented in the devices uses AES-128 per:
The AES-CMAC algorithm is implemented according to:
AES encryption/decryption for authorization sessions uses the GCM AEAD mode per:
RSA signatures are generated and/or verified using the RSASSA-PKCS1-V1_5 scheme
according to the PKCS#1 procedures documented in the following. The exponent is fixed at
0x10001, except for 3072-bit verify, which optionally supports e = 3:
The TA100 device can also calculate and verify RSA
signatures using the RSASSA-PSS schemes according to the PKCS#1 procedures documented
in:
RSA (RSAES-OAEP) encryption and decryption with an exponent of 0x10001 is supported for
1024-bit and 2048-bit key lengths using the RSAES_OAEP PKCS#1 V2.2 scheme documented
in:
Elliptic Curve ECDSA signatures using the NIST curves P224, P256 and P384 are
generated/verified according to the following specification. Keys for all three curves
can be generated using the RNG.
- ANSI X9.62-2005 http://www.ansi.org/
- NIST FIPS 186-5 specification NIST FIPS Publication 186-5
The TA100 device executes the ECDH key agreement according
to NIST Special Publication 800-56A r3 recommendations. All ECDH public and private keys
are treated as ephemeral keys with the corresponding key validation. P224, P256 and P384
curves are supported.
Elliptic Curve computations for the 256-bit Brainpool curve are supported according to
the following document. Sign, verify, key generation and ECDH are all supported. The TA100 device does not support Brainpool curves for X.509
certificate parsing.
ECDSA sign and verify operations are supported for the SECP256K1 curve, often used in
block chain applications. ECDH is not supported for this curve. It is specified in:
The TA100 device supports the TLS 1.2 KDF (PRF), as
specified in:
The TA100 device supports the TLS 1.3 KDF, aka HKDF, as
specified in:
The TA100 device can execute the Burmester-Desmedt
protocol variation of ECDH described at Eurocrypt ’94. Contact Microchip for more
technical details. A version of that paper is available here:
The TA100 device is designed to support the cryptographic
protocols, as specified in:
Microchip uses various evaluation methods to determine the security of the storage
within the device. In this document, the protection level of the private/secret keys
uses the vulnerability analysis in the following JIL document:
Contact Microchip for CAVP certification status of the appropriate cryptographic algorithms.