3 CAM Troubleshooting Guide

The CAM Hardware Driver supports devices with the CAM peripheral. Build failure will occur if the device does not have a CAM peripheral or if there is a mismatch between hardware and library support.

If a build failure occur, ensure the following:

  • The device has a CAM peripheral
  • The latest CAM Hardware Driver is being used
  • The CAM Hardware Driver supports the device (Refer to the table below)
Table 3-1. CAM Hardware Driver Support
Device FamilyCAM Peripheral IDLibrary Name
dsPIC33AK512MPS51205346libcam05346-dspic33a.a