2 Self-Capacitance
Waveform Description
The capacitive self-sensing waveform of the PTC as shown in Fig 2-1 by probing the touch pin with an oscilloscope. The complete PTC acquisition waveform invoking sensor and Cc is shown in Fig 2-2. The Cc waveform cannot be observed by probing.
Operation
Capacitive self-sensing measurements on the Peripheral Touch Controller is done in phases.
* Point 3 is the free space earth to ground return path.
| Phases |
1 Pre-charge |
2 Distribute |
3 Integrate |
4 Discharge |
5 Precharge & Distribute |
6 Integrate |
| Connections |
|
|
|
|
|
|
| Explanation |
Current flows from Vcc to Cx to fully charge the external capacitor.
|
Current flows from Cx to Cc thereby sharing the charge.
|
If Cc and Cx are not same, then the charge proportional to the difference is integrated into Cint. |
Both Cx and Cc are discharged. |
The current flows from Vcc to Cc and Cx, thereby charging both the capacitors (which are in Series). |
If Cc and Cx are not same, then the charge proportional to the difference is integrated into Cint.
The ADC measurement is performed. |
*NC → Not connected
The total charge accumulated on Cint will be proportional to the difference between Cx and Cc.