A USB host or hub supplies nominal 5V power on the VBUS wire for use by USB devices that are
directly connected. In addition, any USB device may have its own power supply. As stated
in the USB 2.0 specification, USB devices that rely solely on power from the USB cable
are called bus-powered devices. In contrast, those having a separate power source
are called self-powered devices.
One important design consideration is the maximum allowed slew rate on the device’s VDD
pin(s). Exceeding this value may cause the device to lock up or even damage the device.
Refer to the Supply Voltage section in the Electrical Characteristics for
details about the power supply's slew rate limits. Because the slew rate of
VBUS can be quite high at the moment the USB is connected, it may be
necessary to include components in the design to reduce the slew rate on the device’s
VDD pin(s). These components will be referred to generically as Slew Rate Limiting
Components or SRLC. These are, for example, power switches with features such as soft
start and reverse blocking.
The USB peripheral’s internal transceiver requires a nominal 3.3V power supply voltage on
the VUSB pin for successful data transfer operations on USB, provided by an
external source or generated by an internal VDD-to-VUSB
(3.3V) voltage regulator called USB VREG. For operating the USB VREG, a minimum
supply voltage VDD ≥ VDDUMIN is required. The USB VREG has
these configuration bits:
The USBVREG bit in the
VUSB Control (VUSBCTRL) register of the SYSCFG peripheral
enables/disables the VUSB regulation.
The USBSINK bit in the
System Configuration 1 (SYSCFG1) fuse controls whether the USB VREG
can sink current. It is recommended to leave this feature enabled.
Refer to the Electrical Characteristics section for standard operating
conditions.
The flexibility of external or internally generated VUSB allows the following
seven power configurations to be supported (with mnemonics in parentheses):
5V Bus-powered (5b)
5V Self-powered (5s)
3.3V Self-powered
(3s)
Dual-powered 5V Bus-dominance and
5V Self-powered (5b5s)
Dual-powered 5V Bus-dominance and
3.3V Self-powered (5b3s)
Dual-powered 5V Bus-dominance and
Self-powered by variable 2V to 3V (5b2s)
Dual-powered 5V Self-dominance
and 5V Bus-powered (5s5b)
5b (5V Bus-powered)
In power configuration 5b, the VBUS supply from the USB receptacle is
connected, either directly or via SRLC, to the device's VDD pin(s). When the USB is
not connected, the device is not powered. When USB is connected, the nominal 5V VBUS
supply powers the device, and the internal voltage regulator must also be enabled,
generating the required 3.3V on the VUSB pin.Figure 6-1. Power Configuration
5b
5s (5V Self-powered)
In power configuration 5s, a local 5V supply is connected, either directly or
via SRLC, to the device's VDD pin(s). Also, enable the internal voltage regulator
while the USB is connected, generating the required 3.3V on the VUSB pin. The
internal voltage regulator may be disabled when the USB is not connected.Figure 6-2. Power Configuration
5s
3s (3.3V Self-powered)
In power configuration 3s, the VDD and VUSB pins are connected, and a local
supply provides 3.3V power to them, either directly or via SRLC. The
internal voltage regulator is unused, and both the USBVREG bit in the
SYSCFG.VUSBCTRL register and the USBSYNC bit in the SYSCFG1 fuse can be
written to `0’.Figure 6-3. Power
Configuration 3s
5b5s (Dual-powered 5V
Bus-dominance and 5V Self-powered)
In power configuration 5b5s, the USB VBUS supply is always used to power the
device when the USB is connected. VBUS is connected, directly or via SRLC,
to the device's VDD pin(s). The internal voltage regulator must also be
enabled, thereby generating the required 3.3V on the VUSB pin. When the USB
is not connected, typically through reverse-blocking circuitry (RBC) such as
a Schottky diode or a transistor configuration, a local 5V supply provides
power to the VDD pin(s). The internal voltage regulator may be disabled when
the USB is not connected by writing the USBVREG bit in the SYSCFG.VUSBCTRL
register to `0’.Figure 6-4. Power
Configuration 5b5s
5b3s (Dual-powered 5V
Bus-dominance and 3.3V Self-powered)
In power configuration 5b3s, the USB VBUS supply is always used to power the
device when the USB is connected. VBUS is connected, directly or via SRLC, to the
device's VDD pin(s). The internal voltage regulator must also be enabled, thereby
generating the required 3.3V on the VUSB pin. A local 3.3V supply provides power to
the VDD pin(s) through RBC when the USB is disconnected. The internal voltage
regulator will be inoperable when the USB is not connected because VDD is
below VDDUMIN.Figure 6-5. Power Configuration
5b3s
5b2s (Dual-powered 5V
Bus-dominance and Self-powered by Variable 2V to 3V)
In power configuration 5b2s, the USB VBUS supply is always used to power the
device when the USB is connected. VBUS is connected, directly or via SRLC, to the
device's VDD pin(s). The internal voltage regulator must also be enabled, generating
the required 3.3V on the VUSB pin. When the USB is not connected, a local supply
that can vary from 2V to 3V, such as a battery, provides power to the device’s VDD
pin(s), typically through RBC. The internal voltage regulator will be inoperable
when the USB is not connected because VDD is below
VDDUMIN.Figure 6-6. Power Configuration
5b2s
5s5b (Dual-powered 5V
Self-dominance and 5V Bus-powered)
In power configuration 5s5b, the device is powered by a local 5V supply
whenever available. The local 5V supply is connected, directly or via SRLC, to the
device's VDD pin(s). If the local supply fails or is unavailable, the device will be
powered only when the USB is connected because VBUS provides power to the device’s
VDD pin(s), typically through RBC. The internal voltage regulator must be enabled
when the USB is connected, generating the required 3.3V on the VUSB pin.Figure 6-7. Power Configuration
5s5b
DS40002548B
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.