2.4 Pin Descriptions
This section contains descriptions of the various LAN8650/1 pins. The “_N” symbol in the signal name indicates that the active, or asserted, state occurs when the signal is at a low voltage level. For example, RESET_N indicates that the reset signal is active low. When “_N” is not present after the signal name, the signal is asserted when at the high voltage level.
The terms assertion and negation are used exclusively. This is done to avoid confusion when working with a mixture of “active low” and “active high” signals. The term assert, or assertion, indicates that a signal is active, independent of whether that level is represented by a high or low voltage. The term negate, or negation, indicates that a signal is inactive.
| Name | Symbol | Buffer Type | Description |
|---|---|---|---|
| Serial Clock | SCLK | VIS-VDDP | Serial clock input |
| Serial Data In | SDI | VIS-VDDP | Serial data input |
| Serial Data Out | SDO | VOH-VDDP | Serial data output |
| Serial Chip Select | CS_N | VIS-VDDP (PU) | Serial peripheral chip select |
| Interrupt | IRQ_N | VO-VDDP (PU) | Device interrupt (Active low) Note: In some cases, the host controllers may require a 10 kΩ (typical) pull-up to its I/O power supply. |
| Name | Symbol | Buffer Type | Description |
|---|---|---|---|
| Ethernet TX/RX Positive Terminal | TRXP | AIO | Positive terminal for transmit/receive signal |
| Ethernet TX/RX Negative Terminal | TRXN | AIO | Negative terminal for transmit/receive signal |
| Name | Symbol | Buffer Type | Description |
|---|---|---|---|
| Inhibit | INH | VODH-VDDAU | Inhibit. Used to switch on/off the main external voltage regulators. This pin operates in the VDDAU domain. RESET_N assertion does not affect the state of this pin. This signal is an active high, P-channel open-drain source output. The pin will be driven to VDDAU to inhibit the shutdown of external voltage regulators. When the external regulators may be shutdown, this pin will become high impedance. Note: When used, this pin requires a pull-down resistor. When not used, this pin should be left unconnected. |
| Wake Input | WAKE_IN | VI-VDDAU | Wakeup Input. Asserted to move the part out of sleep. This pin implements the optional wake input described in the TC10 specification. Note: When used, this pin requires a pull-up or pull-down resistor, depending on the software configured assertion polarity. Note: This pin operates in the VDDAU domain. When not used, this pin should be connected to VSS. |
| Wake Output | WAKE_OUT | VO-VDDP | Wake Output. Asserted when the part wakes out of sleep. This pin implements the optional wake output described in the TC10 specification. Note: When used, this pin requires a pull-down resistor. Note: This pin operates in the VDDP domain. When not used, this pin should be left unconnected. |
| Name | Symbol | Buffer Type | Description |
|---|---|---|---|
Warning: Reserved bits of the pad control register must not be
written with any values other than their default
without instruction from Microchip. | |||
| Configurable Pins | DIOA0 DIOA1 DIOA2 DIOA3 DIOA4 DIOB0 | VIS-VDDP, VO-VDDP |
These pins may be configured as input or output for various purposes. When not used, these pins may be connected directly to ground. |
| Reserved | DIOB1 | This pin is reserved for Microchip test use. It is recommended that this pin is connected directly to ground. | |
| Name | Symbol | Buffer Type | Description |
|---|---|---|---|
| External 25 MHz Crystal Input | XTI | ICLK | External 25 MHz crystal input |
| External 25 MHz Crystal Output | XTO | OCLK | External 25 MHz crystal output |
| System Reset | RESET_N | VIS-VDDP | System reset. This pin is active low. When not used, this pin may be connected directly to VDDP. |
| Bias Resistor | RBIAS | AI | External bias resistor connection pin. This pin requires connection of a 12.4 kΩ resistor to ground. Note: The resistor must be within ± 1% tolerance across the entire expected operating temperature range. |
| Reserved for Test | TEST | VIS-VDDP | This pin should be connected to VDDP. |
| Do Not Connect | DNC | - | The pin must be left floating externally unless otherwise directed by Microchip. |
| Name | Symbol | Description |
|---|---|---|
| Core LDO Supply Compensation | CCOMP | Internal +1.8V LDO core compensation Note: This pin requires a 4.7 μF low ESR capacitor to the PCB ground plane. Note: This pin is only on the LAN8651. |
| +1.8V Switchable Core Power Supply Input | VDDC | +1.8V core power supply input. When in sleep mode, this supply must be disabled. Note: These pins are only on the LAN8650. |
| +3.3V Switchable I/O Power Supply Input | VDDP | +3.3V I/O power supply input. When in sleep mode, this supply must be disabled. |
| +3.3V Continuous VDDAU Power Supply Input | VDDAU | +3.3V continuous VDDAU power supply input. Note: This supply must be provided during sleep mode. Note: When wake/sleep support is not used, this pin is connected to the same supply as VDDA. |
| +3.3V Switchable Analog Power Supply Input | VDDA | +3.3V analog power supply input. When in sleep mode, this supply must be disabled. |
| Ground | VSS | Common ground Note: The exposed pad must be connected to the ground plane with a via array. |