2.4 Pin Descriptions

This section contains descriptions of the various LAN8650/1 pins. The “_N” symbol in the signal name indicates that the active, or asserted, state occurs when the signal is at a low voltage level. For example, RESET_N indicates that the reset signal is active low. When “_N” is not present after the signal name, the signal is asserted when at the high voltage level.

The terms assertion and negation are used exclusively. This is done to avoid confusion when working with a mixture of “active low” and “active high” signals. The term assert, or assertion, indicates that a signal is active, independent of whether that level is represented by a high or low voltage. The term negate, or negation, indicates that a signal is inactive.

Table 2-4. Serial Peripheral Interface (SPI) Pins
NameSymbolBuffer TypeDescription
Serial ClockSCLKVIS‑VDDP

Serial clock input.

This pin is high impedance when the device is in reset.

Serial Data InSDIVIS‑VDDP

Serial data input.

This pin is high impedance when the device is in reset.

Serial Data OutSDOVOH‑VDDP

Serial data output.

This pin is high impedance when the device is in reset.

Serial Chip SelectCS_NVIS‑VDDP (PU)

Serial peripheral chip select.

This pin is high impedance when the device is in reset.

InterruptIRQ_NVO‑VDDP (PU)

Device interrupt (Active low).

This pin is high impedance when the device is in reset.

Note: In some cases, the host controllers may require a 10 kΩ (typical) pull-up to its I/O power supply (VDDP).
Table 2-5. Ethernet Transceiver Pins
NameSymbolBuffer TypeDescription
Ethernet TX/RX Positive 
TerminalTRXPAIO

Positive terminal for transmit/receive signal.

Ethernet TX/RX Negative 
TerminalTRXNAIO

Negative terminal for transmit/receive signal.

Table 2-6. Power Management Pins
NameSymbolBuffer TypeDescription
InhibitINHVODH‑VDDAU

Inhibit. Used to switch on/off the main external voltage regulators.

This pin operates in the VDDAU domain.

RESET_N assertion does not affect the state of this pin.

This signal is an active high, P-channel open-drain source output. The pin will be driven to VDDAU to inhibit the shutdown of external voltage regulators. When the external regulators may be shutdown, this pin will become high impedance.

Note: When used, this pin requires a pull-down resistor.

When not used, this pin should be left unconnected.

Wake InputWAKE_INVI‑VDDAU

Wakeup Input. Asserted to move the part out of sleep. This pin implements the optional wake input described in the TC10 specification.

Note: This pin operates in the VDDAU domain.
Note: When used, this pin requires a pull-up or pull-down resistor, depending on the software configured assertion polarity. If a pull-up is used, it must be connected to VDDAU.

This pin is high impedance when the device is in reset.

When not used, this pin should be connected to VSS.

Wake OutputWAKE_OUTVO‑VDDP

Wake Output. Asserted when the part wakes out of sleep. This pin implements the optional wake output described in the TC10 specification.

This pin is high impedance when the device is in reset.

Note: When used, this pin requires a pull-down resistor.
Note: This pin operates in the VDDP domain.

When not used, this pin should be left unconnected.

Table 2-7. Configurable Pins
NameSymbolBuffer TypeDescription
Warning: Reserved bits of the pad control register must not be written with any values other than their default without instruction from Microchip.
Configurable Pins

DIOA0

DIOA1

DIOA2

DIOA3

DIOA4

DIOB0

VIS‑VDDP, VO‑VDDP

These pins may be configured as input or output for various purposes. When not used, these pins may be connected directly to ground.

These pins are high impedance when the device is in reset.

Reserved

DIOB1

This pin is reserved for Microchip test use. It is recommended that this pin is connected directly to ground.

Table 2-8. Miscellaneous Pins
NameSymbolBuffer TypeDescription
External 25 MHz Crystal InputXTIICLKExternal 25 MHz crystal input.
External 25 MHz Crystal OutputXTOOCLKExternal 25 MHz crystal output.
System ResetRESET_NVIS‑VDDPSystem reset. This pin is active low.

When not used, this pin must be connected directly to VDDP.

Bias
 ResistorRBIASAIExternal bias resistor connection pin. This pin requires connection of a 12.4 kΩ resistor to ground.
Note: The resistor must be within ± 1% tolerance across the entire expected operating temperature range.
Reserved for TestTESTVIS‑VDDPThis pin must be connected to VDDP.
Do Not ConnectDNC—The pin must be left floating externally unless otherwise directed by Microchip.
Table 2-9. Power Pins
NameSymbolDescription
Core LDO Supply CompensationCCOMPInternal +1.8V LDO core compensation.
Note: This pin requires a 4.7 μF low ESR capacitor to the PCB ground plane.
Note: This pin is only on the LAN8651.
+1.8V Switchable Core Power Supply InputVDDC+1.8V core power supply input. When in sleep mode, this supply must be disabled.
Note: These pins are only on the LAN8650.
+3.3V Switchable I/O Power Supply InputVDDP+3.3V I/O power supply input. When in sleep mode, this supply must be disabled.
+3.3V Continuous VDDAU Power 
Supply InputVDDAU+3.3V continuous VDDAU power supply input.
Note: This supply must be provided during sleep mode.
Note: When wake/sleep support is not used, this pin is connected to the same supply as VDDA.
+3.3V Switchable Analog Power 
Supply InputVDDA+3.3V analog power supply input. When in sleep mode, this supply must be disabled.
GroundVSSCommon ground.
Note: The exposed pad must be connected to the ground plane with a via array.