36.3.2.1 UPDI Enabling
Depending on how the application has configured the UPDI pin, one of the following two
methods can be used to enable the UPDI:
- One-Wire Enable - This
method requires the UPDI pin to be configured in UPDI function mode by setting
the UPDIPINCFG bit in the SYSCFG0 register to ‘
1’. - HV Override of UPDI Pin -
This method is used if the UPDI pin is configured in GPIO mode (the UPDIPINCFG
bit in SYSCFG0 is set to ‘
0’). Applying an HV pulse on RESET will reconfigure the UPDI pin to UPDI function mode, thereby overriding the configuration in the SYSCFG0 fuse.