4.2.2 12-bit ADC
12-bit Analog-to-Digital Converter
4.2.2.1 Introduction
This Analog-to-Digital Converter (ADC) module is a 12-bit Successive Approximation Register (SAR) ADC, with a sampling rate up to 130 ksps at a 12-bit resolution. It can be operated in single-ended or differential conversion mode. The ADC input channels are also configurable to use internal peripheral outputs or external analog input pins.
4.2.2.2 Supported Device Families
AVR® Dx | ATtiny | ATmega16xx | ATmega48xx |
AVR®EA | ATmega80x | ATmega88xx |
4.2.2.3 Required header files:
#include "mcc_generated_files/adc/adc[X].h"
4.2.2.4 How to Use the ADC PLIB Driver
The links below provide examples for the different use cases of the ADC Peripheral Library (PLIB) Driver.
General instructions common for all examples: 4.2.2.5.2.1 ADC Use Case Code Snippet Instructions
- 4.2.2.5.2.2 ADC Use Case 1: Basic conversion with Printf An ADC conversion is taken every 100 ms, on the selected analog channel. After each ADC conversion a LED is toggled and the ADC Result is sent to the PC terminal using printf.
- 4.2.2.5.2.3 ADC Use Case 2: Basic mode, with Data Streamer An ADC conversion is taken, on the selected analog channel, every 100 ms. The ADC conversions are triggerd by a timer overflow callback, where the Data Streamer variables adcResult and adcSampleCount are updated.
- 4.2.2.5.2.4 ADC Use Case 2.5: Accumulator mode, with Data Streamer Runs the use case above, with the accumulator and bit shifting, to see the difference that these changes make to the ADC's conversion results.
- 4.2.2.5.2.5 ADC Use Case 3: Windowed ADC, on RTC overflow An ADC conversion is started in a Real-Time Counter (RTC) overflow callback. The ADC is configured in Window mode, only taking samples when < 1v or > 2.5v.
- 4.2.2.5.2.6 ADC Use Case 3.5: Event Triggered ADC Conversions Refactoring the use case above (Windowed ADC, on a 20 ms RTC overflow) to use the Event System (EVSYS) to trigger ADC conversions. Since the EVSYS makes direct hardware connections between the peripherals, the RTC callback (and its registration) can be removed.
- Recommended starting point: UART Driver, Timer/Counter A PLIB Driver and the Data Streamer Library.
- Videos also included for: RTC PLIB Driver, ADC PLIB Driver, AVR Event System.
4.2.2.5 Module Documentation
4.2.2.5.1 ADCx
This file contains the API prototypes and other data types for the ADCx module driver.
Module description
This file contains the API prototypes and other data types for the ADCx module driver.
Typedefs
typedef void(* adc_irq_cb_t) (void)
Function pointer to callback function called by IRQ. NULL=default value: No callback function is to be used.
typedef uint16_t adc_result_t
Data type for the result of non-differential ADC conversion.
typedef int16_t diff_adc_result_t
Data type for the result of differential ADC conversion.
typedef ADC_MUXPOS_t adc_0_channel_t
Data type for the ADC Positive Input Selection.
typedef ADC_MUXNEG_t adc_0_muxneg_channel_t
Data type for the ADC Negative Input Selection.
Enumerations
-
enum ADCx_window_mode_t { ADCx_window_disabled, ADCx_window_below, ADCx_window_above, ADCx_window_inside, ADCx_window_outside }
Window Comparator Modes.
Functions
int8_t ADCx_Initialize (void)
Initializes the ADC. If the module is configured to the Disabled state, the clock to the ADC is disabled as well, if this is supported by the device's clock system.
void ADCx_Enable (void)
Enables the ADC0. If supported by the clock system, it enables the clock of the ADC. Enables the ADC module by setting the Enable bit in the ADC Control register.
void ADCx_Disable (void)
Disables the ADC0. Disables the ADC module by clearing the Enable bit in the ADC Control register. If supported by the clock system, this also disables the clock of the ADC.
void ADCx_EnableAutoTrigger (void)
Enables the conversion auto-trigger.
void ADCx_DisableAutoTrigger (void)
Disables the conversion auto-trigger.
void ADCx_SetWindowHigh (adc_result_t high)
Sets the conversion window comparator high threshold.
void ADCx_SetWindowLow (adc_result_t low)
Sets the conversion window comparator low threshold.
void ADCx_SetWindowMode (ADCx_window_mode_t mode)
Sets the Conversion Window mode.
void ADCx_SetWindowChannel (adc_0_channel_t channel)
Sets the ADC channel to be used for Windowed Conversion mode.
void ADCx_StartConversion (adc_0_channel_t channel)
Starts a conversion on the ADC0.
void ADCx_StartDiffConversion (adc_0_channel_t channel, adc_0_muxneg_channel_t channel1)
Starts a differential conversion on the ADC0.
void ADCx_StopConversion (void)
Stops a conversion on the ADC0.
bool ADCx_IsConversionDone (void)
Checks if the ADC conversion is done.
adc_result_t ADCx_GetConversionResult (void)
Reads a conversion result from the ADC0.
bool ADCx_GetWindowResult (void)
Reads the conversion window result from the ADC0.
adc_result_t ADCx_GetConversion (adc_0_channel_t channel)
Starts a conversion, waits until it is ready, and returns the conversion result.
diff_adc_result_t ADCx_GetDiffConversion (adc_0_channel_t channel, adc_0_muxneg_channel_t channel1)
Starts a differential conversion, waits until ready, and returns the conversion result.
uint8_t ADCx_GetResolution (void)
Returns the number of bits in the ADC conversion result.
void ADCx_RegisterWindowCallback (adc_irq_cb_t f)
Registers a callback function to be called if the conversion satisfies the window criteria.
void ADCx_RegisterResrdyCallback (adc_irq_cb_t f)
Registers a callback function to be called when a measurement is complete and a new result is ready.
Typedef Documentation
adc_0_channel_t
ADC_MUXPOS_t adc_0_channel_t
Data type for the ADC Positive Input Selection.
adc_0_muxneg_channel_t
ADC_MUXNEG_t adc_0_muxneg_channel_t
Data type for the ADC Negative Input Selection.
adc_irq_cb_t
void adc_irq_cb_t
Function pointer to callback function called by IRQ. NULL=default value: No callback function is to be used.
adc_result_t
uint32_t adc_result_t
Data type for the result of non-differential ADC conversion.
diff_adc_result_t
int32_t diff_adc_result_t
Data type for the result of differential ADC conversion.
Function Documentation
ADCx_Disable()
void ADCx_Disable (void )
Disables the ADC0. Disables the ADC module by clearing the Enable bit in the ADC Control register. If supported by the clock system, this also disables the clock of the ADC.
|
None. |
ADCx_DisableAutoTrigger()
void ADCx_DisableAutoTrigger (void )
Disables the conversion auto-trigger.
|
None. |
ADCx_Enable()
void ADCx_Enable (void )
Enables the ADC0. If supported by the clock system, it enables the clock of the ADC. Enables the ADC module by setting the Enable bit in the ADC Control register.
|
None. |
ADCx_EnableAutoTrigger()
void ADCx_EnableAutoTrigger (void )
Enables the conversion auto-trigger.
|
None. |
ADCx_GetConversion()
adc_result_t ADCx_GetConversion (adc_0_channel_t channel)
Starts a conversion, waits until it is ready, and returns the conversion result.
|
adc_result_t - Conversion result read from the ADC0 ADC module. |
ADCx_GetConversionResult()
adc_result_t ADCx_GetConversionResult (void )
Reads a conversion result from the ADC0.
|
adc_result_t - Conversion result read from the ADC0 module. |
ADCx_GetDiffConversion()
diff_adc_result_t ADCx_GetDiffConversion (adc_0_channel_t channel, adc_0_muxneg_channel_t channel1)
Starts a differential conversion, waits until ready, and returns the conversion result.
|
diff_adc_result_t - Conversion result read from the ADC0 ADC module. |
ADCx_GetResolution()
uint8_t ADCx_GetResolution (void )
Returns the number of bits in the ADC conversion result.
|
uint8_t - The number of bits in the ADC conversion result. |
ADCx_GetWindowResult()
bool ADCx_GetWindowResult (void )
Reads the conversion window result from the ADC0.
|
|
ADCx_Initialize()
int8_t ADCx_Initialize (void )
Initializes the ADC. If the module is configured to the Disabled state, the clock to the ADC is disabled as well, if this is supported by the device's clock system.
|
|
ADCx_IsConversionDone()
bool ADCx_IsConversionDone (void )
Checks if the ADC conversion is done.
|
|
ADCx_RegisterResrdyCallback()
void ADCx_RegisterResrdyCallback (adc_irq_cb_t f)
Registers a callback function to be called when a measurement is complete and a new result is ready.
|
None. |
ADCx_RegisterWindowCallback()
void ADCx_RegisterWindowCallback (adc_irq_cb_t f)
Registers a callback function to be called if the conversion satisfies the window criteria.
|
None. |
ADCx_SetWindowChannel()
void ADCx_SetWindowChannel (adc_0_channel_t channel)
Sets the ADC channel to be used for Windowed Conversion mode.
|
None. |
ADCx_SetWindowHigh()
void ADCx_SetWindowHigh (adc_result_t high)
Sets the conversion window comparator high threshold.
|
None. |
ADCx_SetWindowLow()
void ADCx_SetWindowLow (adc_result_t low)
Sets the conversion window comparator low threshold.
|
None. |
ADCx_SetWindowMode()
void ADCx_SetWindowMode (ADCx_window_mode_t mode)
Sets the Conversion Window mode.
|
None. |
ADCx_StartConversion()
void ADCx_StartConversion (adc_0_channel_t channel)
Starts a conversion on the ADC0.
|
None. |
ADCx_StartDiffConversion()
void ADCx_StartDiffConversion (adc_0_channel_t channel, adc_0_muxneg_channel_t channel1)
Starts a differential conversion on the ADC0.
|
None. |
ADCx_StopConversion()
void ADCx_StopConversion (void )
Stops a conversion on the ADC0.
|
None. |
Enumeration Type Documentation
ADCx_window_mode_t
enum ADCx_window_mode_t
Window Comparator Modes.
ADCx_window_disabled |
Window Comparison is Disabled | |
ADCx_window_below |
Result is below a threshold | |
ADCx_window_above |
Result is above a threshold | |
ADCx_window_inside |
Result is inside a window | |
ADCx_window_outside |
Result is outside a window |
4.2.2.5.2 ADC Use Cases
ADC Use Case Code Snippet Instructions
For new users, it is recommended to start with the Timer/Counter A, UART and Data Streamer, since these components are used to support other use cases.
-
Add ADC to the project
-
Configure:
-
The ADCx as described in the example.
-
Any other peripherals or pins needed for the use case.
-
-
Generate the code
-
Add the code snippet(s) to the application code
-
Program the board
ADC Use Case 1: Basic conversion with Printf
An ADC conversion is taken every 100 ms, on the selected analog channel. After each ADC conversion a LED is toggled and the ADC Result is sent to PC terminal using printf.
-
Device Resources:
-
Add ADC
-
Add UART
-
-
Configuration:
-
ADC, Clock Settings:
-
Clock Pre-Scaler: Check ADC Clock (Hz) < 2 Mhz.
-
-
ADC, Hardware Settings:
-
Left Adjust Result: No.
-
Reference select (if no separate VREF component): Select based on analog input (VDD is a good default).
-
-
VREF
-
Enable Force ADC Voltage Reference: Yes.
-
ADC Voltage Reference Source: Select based on analog input (VDD is a good default).
-
-
UART:
-
UART Dependency Selection: Select the UART connected to Serial/CDC port.
-
Redirect STDIO to UART (for printf support): Yes.
-
-
System > Pins, for all pins check board schematics:
-
Pin Grid View: Select an ANx.
-
Pins: Input/Sense Configuration [ISC]: AIx pin (Digital Input buffer disabled).
-
Pin Grid View: Select pin for UART Transmit - Tx.
-
Pin Grid View: Select LED pin as output.
-
Pins: Rename Custom Name to "LED".
-
After configuring the components as described above, click 'Generate' to generate the code. Then add the following code snippets to your application:
#include "mcc_generated_files/system/system.h" #include <util/delay.h>
int main(void) { adc_result_t adcResult; SYSTEM_Initialize(); while(1) { adcResult = ADC0_GetConversion(ADC_MUXPOS_AIN4_gc); //Check the schematic for your board LED_Toggle(); printf("ADC result is: %2d\r\n", adcResult); _delay_ms(100); } }
ADC Use Case 2: Basic mode, with Data Streamer
-
ADC conversions are triggerd by a timer overflow callback, where the Data Streamer variables, adcResult and adcSampleCount, are updated.
-
After each ADC conversion a LED is toggled and SEND_FRAME is set to true, so that a frame is sent to the Data Visualizer from the main while loop.
-
Timer Use Case: 100 ms Timer
-
Data Streamer Use Case: Send Frames at a Period Set by the Timer
-
Device Resources:
-
Add ADC
-
Add Data Streamer
-
Add Timer/Counter A (TCAx)
-
-
Configuration:
-
ADC, Clock Settings:
-
Clock Pre-Scaler: Check ADC Clock (Hz) < 2 Mhz
-
-
ADC, Hardware Settings:
-
Left Adjust Result: No.
-
Reference select (if no separate VREF component): Select based on analog input (VDD is a good default).
-
-
VREF:
-
Enable Force ADC Voltage Reference: Yes
-
ADC Voltage Reference Source: Select based on analog input (VDD is a good default).
-
-
TCAx:
-
Clock Selection: System Clock/x => Select so possible period > needed
-
Requested Timeout(s): 0.1 (100 ms).
-
Enable Overflow Interrupt: Yes
-
-
Data Streamer:
-
UART Dependency Selection: Select the UART connected to Serial/CDC port.
-
-
Data Streamer Table:
-
uint16_t adcResult
-
uint8_t adcSampleCount
-
-
System > Interrupt Manager
-
Global Interrupt Enable: Yes
-
-
System > Pins, for all pins check board schematics:
-
Pin Grid View: Select an ANx.
-
Pins: Input/Sense Configuration [ISC]: AIx pin (Digital Input buffer disabled)
-
Pin Grid View: Select pin for UART Transmit - Tx.
-
Pin Grid View: Select LED pin as output.
-
Pins: Rename Custom Name to "LED".
-
After configuring the components as described above, click 'Generate' to generate the code. Then add the following code snippets to your application:
#include "mcc_generated_files/system/system.h" /* Create a pointer of the type TMR_INTERFACE and assign it to the address of the TCA0_Interface TMR_INTERFACE struct. This enables us to access the portable API interface, which ensures changing the peripheral instance of the timer runs on is easy. */ const struct TMR_INTERFACE *Timer = &TCA0_Interface; volatile bool SEND_FRAME = false;
void Timer_Callback_100ms(void){
DataStreamer.adcResult = ADC0_GetConversion(ADC_MUXPOS_AIN4_gc); //Get the conversion result
DataStreamer.adcSampleCount++;
LED_Toggle();
SEND_FRAME = true;
}
int main(void) { SYSTEM_Initialize(); DataStreamer.adcSampleCount = 0; DataStreamer.adcResult = 0; Timer->TimeoutCallbackRegister(Timer_Callback_100ms); while(1) { if(SEND_FRAME){ WriteFrame(); SEND_FRAME = false; } } }
ADC Use Case 2.5: Accumulator mode, with Data Streamer
Run the use case above, without the accumulator and bit shifting, described below, to see the difference that these changes make to the ADC's conversion results.
-
ADC, Clock Settings:
-
Sample Accumulation Number: 16 (then try with 64)
-
When the accumulator is used, for 16 or more samples, add the following line of code:
void Timer_Callback_100ms(void){ DataStreamer.adcResult = ADC0_GetConversion(ADC_MUXPOS_AIN4_gc); DataStreamer.adcResult = DataStreamer.adcResult >> 4; //Bit shift by 4 for >= 16 accumulated samples DataStreamer.adcSampleCount++; LED_Toggle(); SEND_FRAME = true; }
ADC Use Case 3: Windowed ADC, on RTC overflow
An ADC conversion is started in a Real-Time Counter (RTC) overflow callback. The ADC is configured in Window mode, only taking samples when < 1v or > 2.5v.
-
Device Resources:
-
Add ADC
-
Add Real Time Counter (RTC)
-
Add Data Streamer
-
-
ADC, Hardware Settings:
-
Left Adjust Result: No.
-
Reference select (if no separate VREF component): Select based on analog input (VDD is a good default).
-
-
ADC, Interrupt Settings:
-
Window Comparator Interrupt: Yes.
-
-
ADC, Window Settings:
-
Window Comparator Mode: Outside Window.
-
Enable IRQ on Conversion Satisfying Window Criteria: Yes.
-
Window Comparator High Threshold(V): 2.5(V).
-
Window Comparator Low Threshold(V): 1(V).
-
-
VREF
-
Enable Force ADC Voltage Reference: Yes
-
Select based on analog input (VDD is a good default).
-
-
RTC, Hardware Settings:
-
Period (s): 0.05(s).
-
-
RTC, Interrupt Settings:
-
Overflow Interrupt Enable: Yes.
-
-
Data Streamer:
-
UART Dependency Selection: Select the UART connected to Serial/CDC port.
-
-
Data Streamer Table:
-
uint16_t adcResult
-
uint8_t adcWindowCount
-
-
System > Interrupt Manager
-
Global Interrupt Enable: Yes
-
-
System > Pins, for all pins check board schematics:
-
Pin Grid View: Select an ANx.
-
Pins: Input/Sense Configuration [ISC]: AIx pin (Digital Input buffer disabled)
-
Pin Grid View: Select pin for UART Transmit - Tx.
-
Pin Grid View: Select LED pin as output.
-
Pins: Rename Custom Name to "LED".
-
After configuring the components as described above, click 'Generate' to generate the code. Then add the following code snippets to your application:
#include "mcc_generated_files/system/system.h" volatile bool SEND_FRAME = false;
void Window_Callback(void){ LED_SetLow(); DataStreamer.adcResult = ADC0_GetConversionResult(); DataStreamer.adcWindowCount++; SEND_FRAME = true; } void RTC_Callback(void){ ADC0_StartConversion(ADC_MUXPOS_AIN4_gc); }
int main(void) { SYSTEM_Initialize(); RTC_SetOVFIsrCallback(RTC_Callback); ADC0_RegisterWindowCallback(Window_Callback); DataStreamer.adcResult = 0; DataStreamer.adcWindowCount = 0; while(1) { if(SEND_FRAME){ WriteFrame(); LED_SetHigh(); SEND_FRAME = false; } } }
ADC Use Case 3.5: Event Triggered ADC Conversions
Refactoring the use case above (Windowed ADC on an RTC overflow) to use the Event System (EVSYS) to trigger ADC conversions. Since the EVSYS makes direct hardware connections between the peripherals, the RTC callback (and its registration) can be removed.
Modification of previous use case:
-
Device Resources:
-
Add EVSYS (Event System)
-
-
ADC > Hardware Settings:
-
Positive Input Selection: ADC input pin x //Select based on your schematics
-
Start Event Input Enable: Yes.
-
-
RTC > Hardware Settings:
-
Overflow Interrupt Enable: No.
-
-
EVSYS Configuration:
-
GENERATORS: RTC_OVF -> CHANNELS: CHANNEL0
-
USERS: ADC0START -> CHANNELS: CHANNEL0
-
#include "mcc_generated_files/system/system.h" volatile bool SEND_FRAME = false;
void Window_Callback(void){
LED_SetLow();
DataStreamer.adcResult = ADC0_GetConversionResult();
DataStreamer.adcWindowCount++;
SEND_FRAME = true;
}
int main(void) { SYSTEM_Initialize(); ADC0_RegisterWindowCallback(Window_Callback); DataStreamer.adcResult = 0; DataStreamer.adcWindowCount = 0; while(1) { if(SEND_FRAME){ WriteFrame(); LED_SetHigh(); SEND_FRAME = false; } } }
4.2.2.6 File Documentation
4.2.2.6.1 source/adc.dox File Reference
4.2.2.6.2 source/adc0.c File Reference
API Implementations for ADCx module driver.
#include "../adc0.h"
Functions
int8_t ADCx_Initialize (void)
Initializes the ADC. If the module is configured to the Disabled state, the clock to the ADC is disabled as well, if this is supported by the device's clock system.
void ADCx_Enable (void)
Enables the ADC0. If supported by the clock system, it enables the clock of the ADC. Enables the ADC module by setting the Enable bit in the ADC Control register.
void ADCx_Disable (void)
Disables the ADC0. Disables the ADC module by clearing the Enable bit in the ADC Control register. If supported by the clock system, this also disables the clock of the ADC.
void ADCx_EnableAutoTrigger (void)
Enables the conversion auto-trigger.
void ADCx_DisableAutoTrigger (void)
Disables the conversion auto-trigger.
void ADCx_SetWindowHigh (adc_result_t high)
Sets the conversion window comparator high threshold.
void ADCx_SetWindowLow (adc_result_t low)
Sets the conversion window comparator low threshold.
void ADCx_SetWindowMode (ADCx_window_mode_t mode)
Sets the Conversion Window mode.
void ADCx_SetWindowChannel (adc_0_channel_t channel)
Sets the ADC channel to be used for Windowed Conversion mode.
void ADCx_StartConversion (adc_0_channel_t channel)
Starts a conversion on the ADC0.
void ADCx_StartDiffConversion (adc_0_channel_t channel, adc_0_muxneg_channel_t channel1)
Starts a differential conversion on the ADC0.
void ADCx_StopConversion (void)
Stops a conversion on the ADC0.
bool ADCx_IsConversionDone (void)
Checks if the ADC conversion is done.
adc_result_t ADCx_GetConversionResult (void)
Reads a conversion result from the ADC0.
bool ADCx_GetWindowResult (void)
Reads the conversion window result from the ADC0.
adc_result_t ADCx_GetConversion (adc_0_channel_t channel)
Starts a conversion, waits until it is ready, and returns the conversion result.
diff_adc_result_t ADCx_GetDiffConversion (adc_0_channel_t channel, adc_0_muxneg_channel_t channel1)
Starts a differential conversion, waits until ready, and returns the conversion result.
uint8_t ADCx_GetResolution (void)
Returns the number of bits in the ADC conversion result.
void ADCx_RegisterWindowCallback (adc_irq_cb_t f)
Registers a callback function to be called if the conversion satisfies the window criteria.
void ADCx_RegisterResrdyCallback (adc_irq_cb_t f)
Registers a callback function to be called when a measurement is complete and a new result is ready.
ISR (ADC0_WCMP_vect)
ISR (ADC0_RESRDY_vect)
Variables
adc_irq_cb_t ADCx_window_cb = NULL
adc_irq_cb_t ADCx_resrdy_cb = NULL
Detailed Description
API Implementations for ADCx module driver.
ADC0 Generated Driver File
Function Documentation
ISR()[1/2]
ISR (ADC0_WCMP_vect )
ISR()[2/2]
ISR (ADC0_RESRDY_vect )
Variable Documentation
ADCx_resrdy_cb
adc_irq_cb_t ADCx_resrdy_cb = NULL
ADCx_window_cb
adc_irq_cb_t ADCx_window_cb = NULL
4.2.2.6.3 source/adc0.h File Reference
#include "../system/utils/compiler.h"
Functions
int8_t ADCx_Initialize (void)
Initializes the ADC. If the module is configured to the Disabled state, the clock to the ADC is disabled as well, if this is supported by the device's clock system.
void ADCx_Enable (void)
Enables the ADC0. If supported by the clock system, it enables the clock of the ADC. Enables the ADC module by setting the Enable bit in the ADC Control register.
void ADCx_Disable (void)
Disables the ADC0. Disables the ADC module by clearing the Enable bit in the ADC Control register. If supported by the clock system, this also disables the clock of the ADC.
void ADCx_EnableAutoTrigger (void)
Enables the conversion auto-trigger.
void ADCx_DisableAutoTrigger (void)
Disables the conversion auto-trigger.
void ADCx_SetWindowHigh (adc_result_t high)
Sets the conversion window comparator high threshold.
void ADCx_SetWindowLow (adc_result_t low)
Sets the conversion window comparator low threshold.
void ADCx_SetWindowMode (ADCx_window_mode_t mode)
Sets the Conversion Window mode.
void ADCx_SetWindowChannel (adc_0_channel_t channel)
Sets the ADC channel to be used for Windowed Conversion mode.
void ADCx_StartConversion (adc_0_channel_t channel)
Starts a conversion on the ADC0.
void ADCx_StartDiffConversion (adc_0_channel_t channel, adc_0_muxneg_channel_t channel1)
Starts a differential conversion on the ADC0.
void ADCx_StopConversion (void)
Stops a conversion on the ADC0.
bool ADCx_IsConversionDone (void)
Checks if the ADC conversion is done.
adc_result_t ADCx_GetConversionResult (void)
Reads a conversion result from the ADC0.
bool ADCx_GetWindowResult (void)
Reads the conversion window result from the ADC0.
adc_result_t ADCx_GetConversion (adc_0_channel_t channel)
Starts a conversion, waits until it is ready, and returns the conversion result.
diff_adc_result_t ADCx_GetDiffConversion (adc_0_channel_t channel, adc_0_muxneg_channel_t channel1)
Starts a differential conversion, waits until ready, and returns the conversion result.
uint8_t ADCx_GetResolution (void)
Returns the number of bits in the ADC conversion result.
void ADCx_RegisterWindowCallback (adc_irq_cb_t f)
Registers a callback function to be called if the conversion satisfies the window criteria.
void ADCx_RegisterResrdyCallback (adc_irq_cb_t f)
Registers a callback function to be called when a measurement is complete and a new result is ready.
Typedefs
typedef void(* adc_irq_cb_t) (void)
Function pointer to callback function called by IRQ. NULL=default value: No callback function is to be used.
typedef uint16_t adc_result_t
Data type for the result of non-differential ADC conversion.
typedef int16_t diff_adc_result_t
Data type for the result of differential ADC conversion.
typedef ADC_MUXPOS_t adc_0_channel_t
Data type for the ADC Positive Input Selection.
typedef ADC_MUXNEG_t adc_0_muxneg_channel_t
Data type for the ADC Negative Input Selection.
Enumerations
enum ADCx_window_mode_t { ADCx_window_disabled, ADCx_window_below, ADCx_window_above, ADCx_window_inside, ADCx_window_outside }
Window Comparator Modes.
Detailed Description
ADC0 Generated Driver API Header File