5.3.3 9-byte Config Bits Registers with Secondary XTAL

5.3.3.1 Introduction

The MCC Melody Configuration Bits System Driver generates APIs to support device hardware setup on PIC18F-Q4x target MCUs.

The Configuration settings allow the user to select the oscillators, reset sources and memory protection from the several options available on the device. They are latched in place at the power-up and also after programming of the device.

5.3.3.2 Supported Device Families

PIC18F-Q40PIC18F-Q41

5.3.3.3 Required Header Files:


#include "mcc_generated_files/config_bits.h"

5.3.3.4 Sample Code

Note: The below code is an example code only and the value for each config bit setting will vary depending on the setup on the Configuration Bits module.

//CONFIG1
#pragma config FEXTOSC = ECH     // External Oscillator Mode Selection->EC (external clock) above 8 MHz
#pragma config RSTOSC = EXTOSC     // Power-up Default Value for COSC->EXTOSC operating per FEXTOSC bits (device manufacturing default)

//CONFIG2
#pragma config FCMENP = ON     // Fail-Safe Clock Monitor Enable - Primary XTAL Enable->Fail-Safe Clock Monitor enabled; timer will flag FSCMP bit and OSFIF interrupt on EXTOSC failure.
#pragma config CLKOUTEN = OFF     // Clock Out Enable->CLKOUT function is disabled
#pragma config FCMEN = ON     // Fail-Safe Clock Monitor Enable->Fail-Safe Clock Monitor enabled
#pragma config CSWEN = ON     // Clock Switch Enable->Writing to NOSC and NDIV is allowed
#pragma config FCMENS = ON     // Fail-Safe Clock Monitor Enable - Secondary XTAL Enable->Fail-Safe Clock Monitor enabled; timer will flag FSCMP bit and OSFIF interrupt on SOSC failure.
#pragma config PR1WAY = ON     // PRLOCKED One-Way Set Enable->PRLOCKED bit can be cleared and set only once

//CONFIG3
#pragma config MVECEN = OFF     // Multivector Enable->Interrupt contoller does not use vector table to prioritze interrupts
#pragma config MCLRE = EXTMCLR     // Master Clear (MCLR) Enable->If LVP = 0, MCLR pin is MCLR; If LVP = 1, RE3 pin function is MCLR 
#pragma config BOREN = SBORDIS     // Brown-out Reset Enable->Brown-out Reset enabled , SBOREN bit is ignored
#pragma config PWRTS = PWRT_OFF     // Power-up Timer Selection->PWRT is disabled
#pragma config IVT1WAY = ON     // IVTLOCK One-Way Set Enable->IVTLOCKED bit can be cleared and set only once
#pragma config LPBOREN = OFF     // Low-Power BOR Enable->Low-Power BOR disabled

//CONFIG4
#pragma config XINST = OFF     // Extended Instruction Set Enable->Extended Instruction Set and Indexed Addressing Mode disabled
#pragma config LVP = ON     // Low-Voltage Programming Enable->Low voltage programming enabled. MCLR/VPP pin function is MCLR. MCLRE configuration bit is ignored
#pragma config ZCD = OFF     // ZCD Disable->ZCD module is disabled. ZCD can be enabled by setting the ZCDSEN bit of ZCDCON
#pragma config STVREN = ON     // Stack Overflow/Underflow Reset Enable->Stack full/underflow will cause Reset
#pragma config BORV = VBOR_1P9     // Brown-out Reset Voltage Selection->Brown-out Reset Voltage (VBOR) set to 1.9V
#pragma config PPS1WAY = ON     // PPSLOCKED One-Way Set Enable->PPSLOCKED bit can be cleared and set only once; PPS registers remain locked after one clear/set cycle

//CONFIG5
#pragma config WDTCPS = WDTCPS_31     // WDT Period Select->Divider ratio 1:65536; software control of WDTPS
#pragma config WDTE = OFF     // WDT Operating Mode->WDT Disabled; SWDTEN is ignored

//CONFIG6
#pragma config WDTCWS = WDTCWS_7     // WDT Window Select->window always open (100%); software control; keyed access not required
#pragma config WDTCCS = SC     // WDT Input Clock Selector->Software Control

//CONFIG7
#pragma config SAFEN = OFF     // Storage Area Flash (SAF) Enable->SAF disabled
#pragma config BBEN = OFF     // Boot Block Enable->Boot block disabled
#pragma config BBSIZE = BBSIZE_512     // Boot Block Size Selection->Boot Block size is 512 words
#pragma config DEBUG = OFF     // Debugger Enable->Background Debugger disabled

//CONFIG8
#pragma config WRTB = OFF     // Boot Block Write Protection->Boot Block not Write protected
#pragma config WRTC = OFF     // Configuration Register Write Protection->Configuration registers not Write protected
#pragma config WRTD = OFF     // Data EEPROM Write Protection->Data EEPROM not Write protected
#pragma config WRTAPP = OFF     // Application Block Write Protection->Application Block not write protected
#pragma config WRTSAF = OFF     // Storage Area Flash (SAF) Write Protection->SAF not Write Protected

//CONFIG9
#pragma config CP = OFF     // User Program Flash Memory and Data EEPROM Code Protection->PFM and Data EEPROM code protection disabled


/**
 End of File
*/

5.3.3.5 Module Documentation

5.3.3.5.1 CONFIGBITS Driver

This file contains the API prototypes and other datatypes for the Configuration Bits driver.

Module description

This file contains the API prototypes and other datatypes for the Configuration Bits driver.

Version: Driver Version 2.0.2 Package Version 2.1.6

5.3.3.5.2 System Driver

This file contains the API prototypes and other datatypes for the System Driver.

Module description

This file contains the API prototypes and other datatypes for the System Driver.

Version: Driver Version 2.0.3 Package Version 2.1.6
Functions
  • void SYSTEM_Initialize (void)

    Initializes the system module. This is called only once before calling other APIs.

Function Documentation

SYSTEM_Initialize()

void SYSTEM_Initialize (void )

Initializes the system module. This is called only once before calling other APIs.

Parameters:
None.
Returns:

None.

5.3.3.6 File Documentation

5.3.3.6.1 source/config_bits.c File Reference

This file contains the API Implementation for the Device Configuration Bits driver.

Detailed Description

This file contains the API Implementation for the Device Configuration Bits driver.

CONFIGURATION BITS Generated Driver Source File.

Version: Driver Version 2.0.2 Package Version 2.1.6

5.3.3.6.2 source/config_bits.h File Reference

#include "../system/clock.h"

Detailed Description

Configuration Bits Generated Driver Header File

5.3.3.6.3 source/system.c File Reference

This file contains the API implementation for the System driver.

#include "../system.h"

Functions

  • void SYSTEM_Initialize (void)

    Initializes the system module. This is called only once before calling other APIs.

Detailed Description

This file contains the API implementation for the System driver.

System Driver Source File.

Version: Driver Version 2.0.3 Package Version 2.1.6

5.3.3.6.4 source/system.h File Reference

#include <xc.h>
#include <stdint.h>
#include <stdbool.h>
#include "config_bits.h"
#include "../system/clock.h"
#include "../system/pins.h"
#include "../system/interrupt.h"

Functions

  • void SYSTEM_Initialize (void)

    Initializes the system module. This is called only once before calling other APIs.

Detailed Description

System Driver Header File.