2.4.13 ADCHS_EOSStatusGet Function
C
bool ADCHS_EOSStatusGet(void)
Summary
Returns the status of the end of scan interrupt flag
Description
This function returns the status of the end of scan interrupt flag. End Of Scan (EOS) interrupt is set after the last channel in the scan sequence completes the conversion.
Precondition
ADCHS_Initialize() function must have been called first for the associated instance.
Parameters
None
Returns
false - scan sequence conversion ongoing true - scan sequence conversion is complete
Example
bool ch_status; ADCHS_Initialize(); ADCHS_ModulesEnable(ADCHS_MODULE0_MASK); ADCHS_ConversionStart(); ch_status = ADCHS_EOSStatusGet();
Remarks
None