3.36.7 Digital-to-Analog Converter (DAC)
The Digital-to-Analog Converter (DAC) peripheral provides the following features:
-
Up to two single-ended analog outputs or one differential analog output
-
12-bit resolution
-
Interpolation mode and Dithering mode
Using The Library
The DAC peripheral library provides an interface for the conversion of digital values to analog voltage.
The DAC starts conversion when a new data is loaded into a Data register. The resulting voltage is available on the DAC output after the conversion time.
The user must ensure that new data is not written to the DAC before the last conversion is complete as illustrated below.
// Write new data if DAC is ready if (DAC_IsReady(DAC_CHANNEL_0)) { DAC_DataWrite (DAC_CHANNEL_0, 0xff) }
Library Interface
Digital-to-Analog Converter peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| DAC_Initialize | Initializes DAC module of the device |
| DAC_DataWrite | Converts a Digital data to Analog value |
| DAC_IsReady | Returns the status of readiness of Channel of DAC module for new conversion request |
| DAC_Channel0ResultGet | Returns the Channel 0 Filter output |
| DAC_Channel1ResultGet | Returns the Channel 1 Filter output |
Data types and constants
| Name | Type | Description |
|---|---|---|
| DAC_CHANNEL_NUM | Enum | Identifies the Channel index of DAC module |