3.15.2 Controller Area Network (CAN)
The Controller Area Network with Flexible Data-rate (CAN FD) module supports the following key features:
Standards Compliance:
-
Full CAN 2.0B compliance
-
Programmable bit rate
-
ISO118981:2015 plus CAN FD 1.0 compliant, supports up to 64 data bytes payload/message
-
Arbitration Bit Rate up to one Mbps
-
FD Bit Rate up to eight Mbps Message Reception and Transmission:
-
32 message FIFOs
-
Each FIFO can have up to 32 messages for a total of 512 messages
-
FIFO can be a transmit message FIFO or a receive message FIFO
-
User defined priority levels for message FIFOs used for transmission
-
32 acceptance filters for message filtering
-
32 acceptance filter mask registers for message filtering
-
Automatic response to Remote Transmit Request (RTR)
Using The Library
The CAN library supports the CAN FD and CAN Classic (Normal) mode. The CAN FD and CAN Classic (Normal) mode can transfer message in a polling or an interrupt mode.
CAN FD operation with polling
The following example shows the CAN FD mode operation with polling implementation.
void print_menu(void) { printf("Menu :\\r\\n" " -- Select the action:\\r\\n" " 1: Send FD standard message with ID: 0x45A and 64 byte data 0 to 63. \\r\\n" " 2: Send normal standard message with ID: 0x469 and 8 byte data 0 to \7. \\r\\n" " 3: To receive CAN FD or Normal message \\r\\n" " m: Display menu \\r\\n\\r\\n"); } int main ( void ) { uint32_t messageID = 0; uint32_t rx_messageID = 0; uint32_t status = 0; uint8_t messageLength = 0; uint8_t rx_messageLength = 0; uint8_t count = 0; uint8_t user_input = 0; CANFD_MSG_RX_ATTRIBUTE msgAttr = CANFD_MSG_RX_DATA_FRAME; /* Initialize all modules */ SYS_Initialize ( NULL ); printf(" ------------------------------ \\r\\n"); printf(" CAN FD Demo \\r\\n"); printf(" ------------------------------ \\r\\n"); print_menu(); /* Prepare the message to send*/ for (count = 0; count \< 64; count++) { message[count] = count; } while ( true ) { /* Maintain state machines of all polled Harmony modules. */ /* Check if there is a received character */ if(UART2_ReceiverIsReady() == true) { if(UART2_ErrorGet() == UART_ERROR_NONE) { UART2_Read((void *)&user_input, 1); } switch (user_input) { case '1': printf(" Transmitting CAN FD Message:"); messageID = 0x45A; messageLength = 64; if (CAN1_MessageTransmit(messageID, messageLength, message, 1, CANFD_MODE_FD_WITH_BRS, CANFD_MSG_TX_DATA_FRAME) == true) { printf("Success \\r\\n"); LED_Toggle(); } else { printf("Failed \\r\\n"); } break; case '2': printf(" Transmitting CAN Normal Message:"); messageID = 0x469; messageLength = 8; if (CAN1_MessageTransmit(messageID, messageLength, message, 1, CANFD_MODE_NORMAL, CANFD_MSG_TX_DATA_FRAME) == true) { printf("Success \\r\\n"); LED_Toggle(); } else { printf("Failed \\r\\n"); } break; case '3': printf(" Waiting for message: \\r\\n"); while (true) { if (CAN1_InterruptGet(2, CANFD_FIFO_INTERRUPT_TFNRFNIF_MASK)) { /* Check CAN Status */ status = CAN1_ErrorGet(); if (status == CANFD_ERROR_NONE) { memset(rx_message, 0x00, sizeof(rx_message)); /* Receive New Message */ if (CAN1_MessageReceive(&rx_messageID, &rx_messageLength, rx_message, 0, 2, &msgAttr) == true) { printf(" New Message Received \\r\\n"); status = CAN1_ErrorGet(); if (status == CANFD_ERROR_NONE) { /* Print message to Console */ uint8_t length = rx_messageLength; printf(" Message - ID : 0x%x Length : 0x%x ", (unsigned int) rx_messageID,(unsigned int) rx_messageLength); printf("Message : "); while(length) { printf("0x%x ", rx_message[rx_messageLength - length--]); } printf("\\r\\n"); LED_Toggle(); break; } else { printf("Error in received message"); } } else { printf("Message Reception Failed \\r"); } } else { printf("Error in last received message"); } } } break; default: printf(" Invalid Input \\r\\n"); break; } print_menu(); } } /* Execution should not come here during normal operation */ return ( EXIT_FAILURE ); }
CAN FD operation with interrupt
The following example shows the CAN FD mode operation with interrupt implementation.
/* Application's state machine enum */
typedef enum
{
APP_STATE_CAN_RECEIVE,
APP_STATE_CAN_TRANSMIT,
APP_STATE_CAN_IDLE,
APP_STATE_CAN_USER_INPUT,
APP_STATE_CAN_XFER_SUCCESSFUL,
APP_STATE_CAN_XFER_ERROR
} APP_STATES;
/* Variable to save application state */
static APP_STATES state = APP_STATE_CAN_USER_INPUT;
void APP_CAN_Callback(uintptr_t context)
{
xferContext = context;
/* Check CAN Status */
status = CAN1_ErrorGet();
if ((status & (CANFD_ERROR_TX_RX_WARNING_STATE |
CANFD_ERROR_RX_WARNING_STATE |
CANFD_ERROR_TX_WARNING_STATE | CANFD_ERROR_RX_BUS_PASSIVE_STATE |
CANFD_ERROR_TX_BUS_PASSIVE_STATE | CANFD_ERROR_TX_BUS_OFF_STATE)) ==
CANFD_ERROR_NONE)
{
switch ((APP_STATES)context)
{
case APP_STATE_CAN_RECEIVE:
case APP_STATE_CAN_TRANSMIT:
{
state = APP_STATE_CAN_XFER_SUCCESSFUL;
break;
}
default:
break;
}
}
else
{
state = APP_STATE_CAN_XFER_ERROR;
}
}
int main ( void )
{
uint8_t count = 0;
bool user_input = 0;
/* Initialize all modules */
SYS_Initialize ( NULL );
/* Prepare the message to send*/
messageID = 0x45A;
messageLength = 64;
for (count = 0; count \< 64; count++)
{
message[count] = count;
}
while ( true )
{
if (state == APP_STATE_CAN_USER_INPUT)
{
if(SWITCH_Get() == SWITCH_PRESSED_STATE)
{
while(SWITCH_Get() == SWITCH_PRESSED_STATE);
switch (user_input)
{
case 0:
CAN1_CallbackRegister( APP_CAN_Callback,
(uintptr_t)APP_STATE_CAN_TRANSMIT, 1 );
state = APP_STATE_CAN_IDLE;
CAN1_MessageTransmit(messageID, messageLength, message, 1,
CANFD_MODE_FD_WITH_BRS, CANFD_MSG_TX_DATA_FRAME);
break;
case 1:
CAN1_CallbackRegister( APP_CAN_Callback,
(uintptr_t)APP_STATE_CAN_RECEIVE, 2 );
state = APP_STATE_CAN_IDLE;
memset(rx_message, 0x00, sizeof(rx_message));
/* Receive New Message */
CAN1_MessageReceive(&rx_messageID, &rx_messageLength, rx_message,
0, 2, &msgAttr);
break;
default:
break;
}
}
else
{
continue;
}
}
/* Check the application's current state. */
switch (state)
{
case APP_STATE_CAN_IDLE:
{
/* Application can do other task here */
break;
}
case APP_STATE_CAN_XFER_SUCCESSFUL:
{
if ((APP_STATES)xferContext == APP_STATE_CAN_RECEIVE)
{
}
else if ((APP_STATES)xferContext == APP_STATE_CAN_TRANSMIT)
{
}
LED_Toggle();
state = APP_STATE_CAN_USER_INPUT;
break;
}
case APP_STATE_CAN_XFER_ERROR:
{
if ((APP_STATES)xferContext == APP_STATE_CAN_RECEIVE)
{
}
else
{
}
state = APP_STATE_CAN_USER_INPUT;
break;
}
default:
break;
}
}
/* Execution should not come here during normal operation */
return ( EXIT_FAILURE );
}Library Interface
peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| CANx_Initialize | Initializes given instance of the CAN peripheral |
| CANx_MessageTransmit | Transmits a message into CAN bus |
| CANx_MessageReceive | Receives a message from CAN bus |
| CANx_MessageAbort | Abort request for a FIFO |
| CANx_MessageAcceptanceFilterSet | Set Message acceptance filter configuration |
| CANx_MessageAcceptanceFilterGet | Get Message acceptance filter configuration |
| CANx_MessageAcceptanceFilterMaskSet | Set Message acceptance filter mask configuration |
| CANx_MessageAcceptanceFilterMaskGet | Get Message acceptance filter mask configuration |
| CANx_TransmitEventFIFOElementGet | Get the Transmit Event FIFO Element for the transmitted message |
| CANx_ErrorGet | Returns the error during transfer |
| CANx_ErrorCountGet | Returns the transmit and receive error count during transfer |
| CANx_InterruptGet | Returns the FIFO Interrupt status |
| CANx_TxFIFOQueueIsFull | Returns true if Tx FIFO/Queue is full otherwise false |
| CANx_AutoRTRResponseSet | Set the Auto RTR response for remote transmit request |
| CANx_BitTimingCalculationGet | Returns the bit timing information |
| CANx_BitTimingSet | Sets the bit timing |
| CANx_CallbackRegister | Sets the pointer to the function (and it's context) to be called when the given CAN's transfer events occur |
| CANx_ErrorCallbackRegister | Sets the pointer to the function (and it's context) to be called when error occurs in CAN |
Data types and constants
| Name | Type | Description |
|---|---|---|
| CANFD_MODE | Enum | CANFD Mode for Classic CAN and CAN FD |
| CANFD_MSG_TX_ATTRIBUTE | Enum | CANFD Tx Message Attribute for Tx FIFO and Tx Queue |
| CANFD_MSG_RX_ATTRIBUTE | Enum | CANFD Message RX Attribute for Data Frame and Remote Frame |
| CANFD_FIFO_INTERRUPT_FLAG_MASK | Enum | CANFD FIFO Interrupt Status Flag Mask |
| CANFD_ERROR | Enum | CANFD Transfer Error data type |
| CANFD_CALLBACK | Typedef | CANFD Callback Function Pointer |
| CANFD_RX_MSG | Struct | CANFD RX Message Buffer structure |
| CANFD_RX_MSG_OBJECT | Struct | CANFD Receive Message Object structure |
| CANFD_TX_MSG_OBJECT | Struct | CANFD Transmit Message Object structure |
| CANFD_TX_EVENT_FIFO_ELEMENT | Struct | CANFD Trasmit Event FIFO Element structure |
| CAN_NOMINAL_BIT_TIMING | Struct | Nominal bit timing parameters |
| CAN_BIT_TIMING | Struct | Bit timing parameters |