1.3 Configuring an Ordinary PTP Slave Clock using Web GUI

To configure an ordinary PTP slave clock, perform the following steps:

  1. Click Configuration > PTP.
  2. Click Add New PTP Clock.
  3. Configure the following properties:
    1. HW Domain = 0
    2. Device Type = Slaveonly
    3. Profile = 1588
    Figure 1-6. Create PTP Slave Clock Instance
  4. Click Save.
  5. Click the Clock Instance link.
    Figure 1-7. Select PTP Clock Instance
  6. The PTP Clock’s Configuration and Status page opens. Configure the following properties:
    1. Under the Port Enable and Configuration area, select the suitable ports.
    2. Under the Clock Default Dataset area, set the following:
      1. From the 2 Step Flag drop-down list, select True.
      2. In the Pri1 text box, type a lower number than the PTP slave.
    3. Under Port Enable and Configuration area, click Ports Configuration. The PTP clock’s Port Data Set Configuration page opens.
    Figure 1-8. Configure PTP Slave Clock Instance
  7. To set delay mechanism used in the path, in the Dlm box, type or select suitable value, and then click Save.
    Figure 1-9. Configure Port Data for PTP Slave Clock Instance
  8. Check for Phase_Locked status and verify the PTP clock offset from the PTP master.
    Figure 1-10. Configure PTP Clock's Configuration