9.1 Generating FRER using Web GUI

To generate FRER, perform the following steps:

  1. To enable VLAN hybrid on both Ingress and Egress ports, see Time Aware Shaper.
  2. Click TSN > Streams. The Stream Configuration page opens.
    Figure 9-2. Stream Configuration
  3. To add a stream, click + .
  4. Click TSN > FRER. The FRER Configuration page opens. On the configuration page, perform the following:
    1. Press +.
    2. To set mode, in the Mode list, click Generation.
    3. Configure Instance, FRER VLAN, Ingress Stream List, and Egress Stream List, as shown in the following figure.
    4. To enable FRER, select the Enable check box.
    5. Click Save.
    Figure 9-3. FRER Configuration