9.3 Recovering FRER using Web GUI
To recover FRER, perform the following steps:
- To enable VLAN hybrid on both Ingress and Egress ports, see Time Aware Shaper.
- Click TSN > Streams. The Stream Configuration page opens.
- To add a stream, click + .
- Click TSN > FRER.
The FRER Configuration page opens. On the configuration page, perform the
following:
- Press +.
- To set mode to Recovery, in the Mode list, click Recovery.
- Configure Instance, FRER VLAN, Ingress Stream List, and Egress Stream List, as shown in the following figure.
- To enable FRER, select the Enable check box.
- Click Save.