10.1 Configuring SyncE using Web GUI

To configure SyncE, perform the following steps:

  1. Click Configuration > SyncE.
  2. In the Clock Source and State, ensure the following:
    1. Check the Nominated Clock source.
    2. Select the nominated port.
  3. In the Clock Selection Mode and State table, ensure the following:
    1. Make sure the the source is the same as the nominated clock source.
    2. Set WTR Time to disable.
  4. In the SyncE Ports table, check the ports that are in use with SyncE.
  5. Make sure that LOCS, LOL and DHOLD becomes Green.
  6. Make sure that under the Clock Selection Mode and State section, State becomes Locked.
Figure 10-1. SyncE Configuration
Note: For a more detailed SyncE configuration guide, go to SyncE Software Configuration Guide (microchip.com).