6.1 Configuring QoS Egress Port Schedulers using Web GUI

To configure the QoS egress port schedulers, perform the following steps:

  1. To enable Tag Class on the Ergress Port and to enable VLAN hybrid on both Ingress & Egress ports, see Time Aware Shaper.
  2. Click QOS > Port Scheduler. The QoS Egress Port Schedulers page opens.
    Figure 6-1. QoS Egress Port Scheduler
    A screenshot of a computer screen Description automatically generated
  3. Click the port (Port 2 is considered) to be configured . The QoS Egress Port Scheduler and Shapers Port 2 page opens.
    Figure 6-2. QoS Egress Port Scheduler and Shapers Port 2
  4. Select the Cut-through check box for the Egress port.
  5. Click Save.