1.7 Configuring an End-to-End Transparent Clock using Web GUI
To configure an end-to-end transparent clock, perform the following steps:
- Click Configuration > PTP.
- Click Add New PTP Clock.
- Configure the following properties:
- HW Domain = 0
- Device Type = P2pTransp
- Profile = 1588
- Click Save.
- In the PTP External Clock Mode page (see the following figure), click the Clock Instance link. The PTP Clock’s Port Configuration and Status page opens.
- Configure the following properties:
- Under the Port Enable and Configuration area, select the suitable ports.
- From the 2 Step Flag list, click TRUE.
- In the Pri1 box, type a lower number than the PTP slave.
- Click the Port Configuration link. The PTP Clock’s Port Data Set Configuration page opens.
- In the Dlm box, click e2e, and then click Save.
- Ensure that the Slave State column is set to FREERUN in the Clock Current DataSet table.