12.6 Accessing Elements in SIMD Variables
The use of SIMD variables enables operations on multiple data in parallel. However, in certain situations, programmers need to access elements inside a SIMD variable. This can be done by using a union type that unites a SIMD type and an array of a basic type as follows.
typedef union
{
v4i8 a;
unsigned char b[4];
} v4i8_union;
typedef short q15;
typedef union
{
v2q15 a;
q15 b[2];
} v2q15_union;
As shown in the figure above for a v4i8 variable, b[0]
is used to access the first element in the variable. The element b[0]
is right-most position. The following examples show how to extract or assign elements.
Example:
/* v4i8 Example */
v4i8 i;
unsigned char j, k, l, m;
v4i8_union temp;
/* Assume we want to extract from i. */
temp.a = i;
j = temp.b[0];
k = temp.b[1];
l = temp.b[2];
m = temp.b[3];
/* Assume we want to assign j, k, l, m to i. */
temp.b[0] = j;
temp.b[1] = k;
temp.b[2] = l;
temp.b[3] = m;
i = temp.a;
/* -------------------------------------------------------- */
Example:
/* v2q15 Example */
v2q15 i;
q15 j, k;
v2q15_union temp;
/* Assume we want to extract from i. */
temp.a = i;
j = temp.b[0];
k = temp.b[1];
/* Assume we want to assign j, k to i. */
temp.b[0] = j;
temp.b[1] = k;
i = temp.a;
Using SIMD data types is a very powerful technique. Programmers can enjoy the performance improvement from SIMD data types by calling the DSP built-in functions (see Built-In Functions) and/or using generic C operators. For SIMD data types, the compiler can map C operators (e.g., +, -, *, /) to hardware instructions directly, so long as the selected target PIC32 MCU features the DSP-enhanced core.
Here are some examples:
typedef signed char v4i8 __attribute__ ((vector_size(4)));
v4i8 a, b, c;
c = a + b; // compiler generates addu.qb
c = a - b; // compiler generates subu.qb
/* -------------------------------------------------------- */
typedef short v2q15 __attribute__ ((vector_size(4)));
v2q15 d, e, f;
f = d + e; // compiler generates addq.ph
f = d - e; // compiler generates subq.ph
/* -------------------------------------------------------- */
typedef short v2i16 __attribute__ ((vector_size(4)));
v2i16 x, y, z;
z = x * y; // compiler generates mul.ph
/* -------------------------------------------------------- */
typedef _Sat _Fract sat_v2hq __attribute__ ((vector_size(4)));
sat_v2hq a, b, c;
c = a + b; // compiler generates addq_s.ph
c = a - b; // compiler generates subq_s.ph
c = a * b; // compiler generates mulq_rs.ph