24.3 Data Type

Some compilers allow use of the boolean type, bool, as well as associated values true and false, as specified by the C99 C Language Standard. This type and these values may be used by all MPLAB XC compilers when in compatibility mode (see note), as shown in the table below.

As indicated by the Standard, the <stdbool.h> header must be included for this feature to work as expected when it is used with MPLAB XC compilers.

Table 24-3. Support for C99 Bool Type
IAR Compatibility Mode
TypeXC16/XC-DSCXC32
boolsupportsupport
Note: Not all C99 features have been adopted by all Microchip MPLAB XC compilers.