10.2.2 Static Variables
All static
variables have permanent storage duration, even those defined
inside a function which are “local static” variables. Local static
variables only have scope in the function or block in which they are defined, but unlike
auto
variables, their memory is reserved for the entire duration of
the program. Thus, they are allocated memory like other non-auto
variables. Static variables may be accessed by other functions via pointers, since they
have permanent duration.
Variables which are static
are guaranteed to retain their value between
calls to a function, unless explicitly modified via a pointer.
Variables which are static
and initialized have their
initial value assigned only once during the program's execution. Thus, they may be
preferable over initialized auto
objects which are assigned a value
every time the block they are defined in begins execution. Any initialized static
variables are initialized in the same way as other non-auto
initialized
objects by the runtime start-up code, see Peripheral Library Functions. Static variables
are located in the same sections as their non-static
counterparts.