16.2.1 Function Attributes
address(addr)
The address attribute specifies an absolute physical address at which the attributed routine will be placed in memory. It can be used with C and C++ functions.
address attribute specifies an absolute virtual address for the function. Be
sure to specify the address attribute using an appropriate virtual address
for the target device. The address is typically in the range [0x9D000000,0x9D0FFFFC], as
defined in the linker script as the kseg0_program_mem memory region. For
example:__attribute__((address(0x9D008000))) void bar (void);The compiler performs no error checking on the address. The section containing the function will be located at the specified address regardless of the memory-regions specified in the linker script or the actual memory ranges on the target device. The application code must ensure that the address is valid for the target device.
To make effective use of absolute sections and the new best-fit allocator, standard program-memory and data-memory sections should not be mapped in the linker script. The built-in linker script does not map most standard sections such as the .text, .data, .bss, or .ramfunc sections. By not mapping these sections in the linker script, we allow these sections to be allocated using the best-fit allocator rather than the sequential allocator. Sections that are unmapped in the linker script can flow around absolute sections, whereas sections that are linker-script mapped are grouped together and allocated sequentially, potentially causing conflicts with absolute sections.
alias ("symbol")
Indicates that the function is an alias for another symbol. For example:
void foo (void) { /* stuff */ }
__attribute__ ((alias("foo"))) void bar (void);Symbol bar is considered to be an alias for the symbol foo.
always_inline
If the function is declared inline, always inline the function, even if no optimization level was specified.
at_vector
Place the body of the function at the indicated exception vector address.
See Interrupts and Exception Handlers.
const
If a pure function determines its return value exclusively from its parameters (that is, does not examine any global variables), it may be declared const, allowing for even more aggressive optimization. Note that a function which de-references a pointer argument is not const since the pointer de-reference uses a value which is not a parameter, even though the pointer itself is a parameter.
deprecated
deprecated (msg)
When a function specified as deprecated is used, a warning is generated. The optional msg argument, which must be a string, will be printed in the warning if present. The deprecated attribute may also be used for variables and types.
externally_visible
This attribute when used with a function, nullifies the effect of the -fwhole-program command-line option, so the function remains visible outside the current compilation unit. This might prevent certain optimizations from being performed on the function.
far
Always invoke the function by first loading its address into a register and then using the contents of that register. This allows calling a function located beyond the 28-bit addressing range of the direct CALL instruction.
format (type, format_index, first_to_check)
The format attribute indicates that the function takes a printf, scanf, strftime, or strfmon style format string and arguments and that the compiler should type check those arguments against the format string, just as it does for the standard library functions.
The type parameter is one of printf, scanf, strftime or strfmon (optionally with surrounding double underscores, for example, __printf__) and determines how the format string will be interpreted.
The format_index parameter specifies which function parameter is the format string. Function parameters are numbered from the left-most parameter, starting from 1.
The first_to_check parameter specifies which parameter is the first to check against the format string. If first_to_check is zero, type checking is not performed and the compiler only checks the format string for consistency (for example, vfprintf).
format_arg (index)
The format_arg attribute specifies that a function manipulates a printf style format string and that the compiler should check the format string for consistency. The function attribute which is a format string is identified by index.
function_replacement_prologue
This feature allows the application to redirect one function to another implementation at runtime without replacing the existing function. This is achieved by changing the method of invoking functions through a function replacement table instead of from a linker-resolved address. Initially the function address in the table points to the location of the entry point of the original function's prologue. The application can then replace the table entry with the new function address. Now, during the program execution, the control will pass to the new function address and returns to the caller function. This feature adds a new function_replacement_prologue function attribute. To redirect the function, modify the corresponding Function Replacement Table entry at runtime.
Example C code:
int a, b, c, d;
int __attribute__((function_replacement_prologue)) foo (void)
{
a = b + c;
return (a);
}
int main()
{
d = foo();
return 0;
}Example generated assembly code:
# Function Replacement Table entries, located in data memory
.section .fixtable, data
fixtable.foo:
.word cont.foo # By default, populate the table with the address
# of the original implementation. Redirect to
# another implementation by overwriting this
# location with the address of the new implementation.
.section .text, code
.globl foo
.ent foo
.type foo, @function
foo:
# Begin Function Replacement Table Prologue
lui $25,%hi(fixtable.foo) # Load address from .fixtable above
lw $25,%lo(fixtable.foo)($25)
j $25 # Jump to address loaded from table
nop
cont.foo:
# End Function Replacement Table Prologue
addiu $sp,$sp,-8
sw $fp,4($sp)
move $fp,$sp
lw $3,%gp_rel(b)($28)
...........
j $31
nopinterrupt (priority)
Generate prologue and epilogue code for the function as an interrupt handler function. See Interrupts . The argument specified the interrupt priority level using the symbols IPLnSOFT, IPLnSRS, or IPLnAUTO where n represents the 7 levels of priority and SOFT|SRS|AUTO specifies the context saving mode.
keep
The __attribute__((keep)) may be applied to a function. The keep attribute will prevent the linker from removing the function with --gc-sections, even if it is unused.
void __attribute__((keep)) foo(void);
longcall
Functionally equivalent to far.
malloc
Any non-Null Pointer return value from the indicated function will not alias any other pointer which is live at the point when the function returns. This allows the compiler to improve optimization.
micromips
Generate code for the function in the compressed microMIPS instruction set.
mips16
Generate code for the function in the MIPS16 instruction set.
naked
Generate no prologue or epilogue code for the function. This attribute is intended for functions that exclusively contain extended inline assembly code. Using C code within such an attributed function might not work properly. Since the compiler will not generate prologue or epilogue code for functions using this attribute, the application code within is responsible for managing the stack and additionally handling formal parameters, return values, and the function return.
near
Always invoke the function with an absolute CALL instruction, even when the -mlong-calls command line option is specified.
no_fpu
The no_fpu attribute must be used in conjunction with the interrupt (priority) attribute and specifies that the interrupt service routine (ISR) should not preserve the Floating-Point Unit (FPU) context. In addition it causes the compiler to insert code into the ISR that will disable the FPU, by clearing the CU1 bit of the CP0 Status register. If your ISR attempts to perform floating-point operations while the FPU is disabled, the device will trigger a general exception. This also means that any higher-priority ISR interrupting an ISR using the no_fpu attribute must re-enable the FPU if floating-point operations are required. The ISR restores the original value of the status register before returning from the interrupt.
noinline
The function will never be considered for inlining.
noload
Causes the variable or function to be placed in a section that has the noload attribute set. It tells consumers of the ELF files not to load the contents of the section. This attribute can be useful when you just want to reserve memory for something, but you don’t want to clear or initialize memory.
void bar() _ attribute_ ((noload))
nomips16
Always generate code for the function in the MIPS32® instruction set, even when compiling the translation unit with the -mips16 command line option.
nonnull (index, ...)
Indicate to the compiler that one or more pointer arguments to the function must be non-null. If the compiler determines that a Null Pointer is passed as a value to a non-null argument, and the -Wnonnull command line option was specified, a warning diagnostic is issued.
If no arguments are given to the nonnull attribute, all pointer arguments of the function are marked as non-null.
noreturn
Indicate to the compiler that the function will never return. In some situations, this can allow the compiler to generate more efficient code in the calling function since optimizations can be performed without regard to behavior if the function ever did return. Functions declared as noreturn should always have a return type of void.
optimize(optimization)
optimize attribute allows a function to be built with optimizations that
differ from what has been specified on the command line and which will be applied to the rest
of the program. The optimization argument can either be a
number or a string. String arguments represent the command-line option used to control an
optimization, for example, to enable peephole optimizations (-fpeephole), use
optimize("peephole"). The -f option prefix does not need
to be specified with the argument. If you want to specify more than one optimization, separate
the arguments with commas but with no space characters. Arguments that begin with
O are assumed to be an optimization level option, for example
optimize("O1,unroll-loops") turns on level 1 optimizations and the
unroll-loops optimizations (controlled by the -funroll-loops command-line
option). A numerical argument is also assumed to be an optimization level, for example
optimize(3) turns on level 3 optimizations and is equivalent to the full
usage of the attribute in the following example.
int __attribute__((optimize("O3"))) pandora (void) {
if (maya > axton)
return 1;
return 0;
}This
feature can be used, for instance, to have frequently executed functions compiled with more
aggressive optimization options that produce faster and larger code, while other functions can
be called with less aggressive options. Typically, however, it is not used for production
builds.pure
If a function has no side effects other than its return value, and the return value is dependent only on parameters and/or (nonvolatile) global variables, the compiler can perform more aggressive optimizations around invocations of that function. Such functions can be indicated with the pure attribute.
ramfunc
The ramfunc attribute locates the attributed routine in RAM rather than in
Flash memory on devices that normally execute code from Flash. This attribute can be used for
both C functions and C++ class methods. The compiler's default runtime startup code uses the
data-initialization template to copy the code associated with functions using this attribute
from Flash to RAM at program startup.
When this attribute is used with C functions, the function is placed at the highest appropriately
aligned address for executable code. Note that due to ramfunc alignment and
placement requirements, the address attribute should not be used with the
ramfunc attribute. The presence of the ramfunc section
causes the linker to emit the symbols necessary for the crt0.S start-up
code to initialize the bus matrix appropriately for executing code out of data memory.
far/longcall attribute and the
section attribute. For
example: __attribute__((ramfunc,section(".ramfunc"),far,unique_section))
unsigned int myramfunct (void_
{ /* code */ }<sys/attribs.h> header file makes the ramfunc
attribute simple to
use: #include <sys/attribs.h>
__longramfunc__ unsigned int myramfunct (void)
{ /* code */ }class printmyname {
// Access specifier
public:
// Data Members
string myname;
int dummy ;
// Member Functions()
printmyname (){
myname = "microchip";
}
void __attribute__((ramfunc, long_call)) set_name(string newname){
myname = newname;
dummy = 9;
}
void printname() { cout << "name is:" << myname; }
};section("name")
Place the function into the named section.
For example:
void __attribute__ ((section (".wilma"))) baz () {return;}
Function baz will be placed in section .wilma.
The -ffunction-sections command line option has no effect on functions defined with a section attribute.
unique_section
Place the function in a uniquely named section, as if -ffunction-sections had been specified. If the function also has a section attribute, use that section name as the prefix for generating the unique section name.
For example:
void __attribute__ ((section (".fred"), unique_section) foo (void) {return;}
Function foo will be placed in section .fred.foo.
unused
Indicate to the compiler that the function may not be used. The compiler will not issue a warning for this function if it is not used.
used
Indicate to the compiler that the function is always used and code must be generated for the function even if the compiler cannot see a reference to the function. For example, if inline assembly is the only reference to a static function.
vector (num)
Generate a branch instruction at the indicated exception vector which targets the function. See Interrupts and Exception Handlers.
warn_unused_result
A warning will be issued if the return value of the indicated function is unused by a caller.
weak
A weak symbol indicates that if another version of the same symbol is available, that version should be used instead. For example, this is useful when a library function is implemented such that it can be overridden by a user written function.