4.4 Project Setup
To set up an MPLAB X IDE project for the first time, use the built-in Project Wizard (File>New Project). In this wizard, you will be able to select a language toolsuite that uses the 32-bit language tools. For more on the wizard, and MPLAB X IDE projects, see MPLAB X IDE documentation.
Once you have a project set up, you may then set up properties of the tools in MPLAB X IDE.
- From the MPLAB X IDE menu bar, select File>Project Properties to open a window to set/check project build options.
- Under “Conf:[default]”, select a tool from the tool collection to set up.