5 Command-line Driver
The MPLAB XC32 C Compiler command-line
driver, , can be invoked to perform all aspects
of compilation, including C code generation, assembly and link steps. Its use is the
recommended way to invoke the compiler, as it hides the complexity of all the internal
applications and provides a consistent interface for all compilation steps. Even if an IDE
is used to assist with compilation, the IDE will ultimately call xc32-gccxc32-gcc.
If you are developing a project that contains
C++ source code, an alternate driver called xc32-g++ is supplied and that will link in an alternate set of
libraries. Its operation is similar to the xc32-gcc driver.
This chapter describes the steps that the driver takes during compilation, the files that the driver can accept and produce, as well as the command-line options that control the compiler’s operation.